Cyclic Redundancy Check#

Introduction#

The Cyclic Redundancy Check (CRC) in embedded systems identifies inadvertent data changes. It generates a checksum, which is applied to the data before transmission or storage. When data is received or retrieved, the CRC is recalculated and compared to the original checksum to confirm its integrity.

Configuration#

Configuring CRC typically involves several parameters like below:

  • Modify SL_CRC_POLYNOMIAL to set the desired polynomial value.

  • Modify SL_CRC_POLY_WIDTH to set the desired polynomial width.

Usage#

The common CRC functions can be used after the CRC Structures are specified, passing an instance of sl_crc_params_t. The following functions will initiate and configure the CRC below, which is the flow for implementation.

  1. sl_si91x_crc_set_gen_control

  2. sl_si91x_crc_enable

  3. sl_si91x_crc_polynomial

  4. sl_si91x_crc_polynomial_width

  5. sl_si91x_crc_lfsr_init

  6. sl_si91x_crc_use_swapped_init

  7. sl_si91x_crc_set_data_width_type

  8. sl_si91x_crc_set_fifo_thresholds

  9. sl_si91x_crc_monitor_crc_calc

  10. sl_si91x_crc_disable

Typedefs#

typedef RSI_CRC_PARAMS_T

Renamed CRC param structure.

Functions#

sl_status_t
sl_si91x_crc_get_general_status(uint32_t *reg_status)
sl_status_t
sl_si91x_crc_polynomial(sl_crc_params_t *pCRCParams)
sl_status_t
sl_si91x_crc_polynomial_width(sl_crc_params_t *pCRCParams, uint32_t *reg_status)
sl_status_t
sl_si91x_crc_lfsr_init(sl_crc_params_t *pCRCParams)
sl_status_t
sl_si91x_crc_use_swapped_init(sl_crc_params_t *pCRCParams, uint32_t *reg_status)
sl_status_t
sl_si91x_crc_set_data_width_type(sl_crc_params_t *pCRCParams, uint32_t *oper_status)
sl_status_t
sl_si91x_crc_set_fifo_thresholds(sl_crc_params_t *pCRCParams, uint32_t *oper_status)
sl_status_t
sl_si91x_crc_write_data(sl_crc_params_t *pCRCParams, uint32_t data, uint32_t *oper_status)
sl_status_t
sl_si91x_crc_monitor_crc_calc(sl_crc_params_t *pCRCParams, uint32_t *crc)
sl_status_t
sl_si91x_crc_lfsr_dynamic_write(sl_crc_params_t *pCRCParams)
sl_status_t
sl_status_t
sl_si91x_crc_get_fifo_status(uint32_t *reg_status)
sl_status_t

Enables the CRC peripheral.

sl_status_t

Disable the CRC peripheral.

Macros#

#define

Polynomial used for CRC calculation.

#define

Width of the polynomial.

#define

Initial LFSR value.

#define

Width type of the CRC.

#define

Width of the input data.

#define

Number of bytes to be written to the CRC.

#define

Almost empty threshold level.

#define

Almost full threshold level.

#define

Whether to swap the input data.

#define

Whether to use uDMA for CRC calculation.

#define

Whether to swap the LFSR value.

Typedef Documentation#

sl_crc_params_t#

typedef RSI_CRC_PARAMS_T sl_crc_params_t

Renamed CRC param structure.


Function Documentation#

sl_si91x_crc_set_gen_control#

sl_status_t sl_si91x_crc_set_gen_control (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

sl_si91x_crc_get_general_status#

sl_status_t sl_si91x_crc_get_general_status (uint32_t * reg_status)
Parameters
TypeDirectionArgument NameDescription
uint32_t *N/Areg_status

sl_si91x_crc_polynomial#

sl_status_t sl_si91x_crc_polynomial (sl_crc_params_t * pCRCParams)
Parameters
TypeDirectionArgument NameDescription
sl_crc_params_t *N/ApCRCParams

sl_si91x_crc_polynomial_width#

sl_status_t sl_si91x_crc_polynomial_width (sl_crc_params_t * pCRCParams, uint32_t * reg_status)
Parameters
TypeDirectionArgument NameDescription
sl_crc_params_t *N/ApCRCParams
uint32_t *N/Areg_status

sl_si91x_crc_lfsr_init#

sl_status_t sl_si91x_crc_lfsr_init (sl_crc_params_t * pCRCParams)
Parameters
TypeDirectionArgument NameDescription
sl_crc_params_t *N/ApCRCParams

sl_si91x_crc_use_swapped_init#

sl_status_t sl_si91x_crc_use_swapped_init (sl_crc_params_t * pCRCParams, uint32_t * reg_status)
Parameters
TypeDirectionArgument NameDescription
sl_crc_params_t *N/ApCRCParams
uint32_t *N/Areg_status

sl_si91x_crc_set_data_width_type#

sl_status_t sl_si91x_crc_set_data_width_type (sl_crc_params_t * pCRCParams, uint32_t * oper_status)
Parameters
TypeDirectionArgument NameDescription
sl_crc_params_t *N/ApCRCParams
uint32_t *N/Aoper_status

sl_si91x_crc_set_fifo_thresholds#

sl_status_t sl_si91x_crc_set_fifo_thresholds (sl_crc_params_t * pCRCParams, uint32_t * oper_status)
Parameters
TypeDirectionArgument NameDescription
sl_crc_params_t *N/ApCRCParams
uint32_t *N/Aoper_status

sl_si91x_crc_write_data#

sl_status_t sl_si91x_crc_write_data (sl_crc_params_t * pCRCParams, uint32_t data, uint32_t * oper_status)
Parameters
TypeDirectionArgument NameDescription
sl_crc_params_t *N/ApCRCParams
uint32_tN/Adata
uint32_t *N/Aoper_status

sl_si91x_crc_monitor_crc_calc#

sl_status_t sl_si91x_crc_monitor_crc_calc (sl_crc_params_t * pCRCParams, uint32_t * crc)
Parameters
TypeDirectionArgument NameDescription
sl_crc_params_t *N/ApCRCParams
uint32_t *N/Acrc

sl_si91x_crc_lfsr_dynamic_write#

sl_status_t sl_si91x_crc_lfsr_dynamic_write (sl_crc_params_t * pCRCParams)
Parameters
TypeDirectionArgument NameDescription
sl_crc_params_t *N/ApCRCParams

sl_si91x_crc_reset_fifo#

sl_status_t sl_si91x_crc_reset_fifo (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

sl_si91x_crc_get_fifo_status#

sl_status_t sl_si91x_crc_get_fifo_status (uint32_t * reg_status)
Parameters
TypeDirectionArgument NameDescription
uint32_t *N/Areg_status

sl_si91x_crc_enable#

sl_status_t sl_si91x_crc_enable (void )

Enables the CRC peripheral.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function enables the CRC peripheral by enabling its clock.

Returns

  • status 0 if successful, else error code as follow

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid.


sl_si91x_crc_disable#

sl_status_t sl_si91x_crc_disable (void )

Disable the CRC peripheral.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function Disables the CRC peripheral by disabling its clock.

Returns

  • status 0 if successful, else error code as follow

    • SL_STATUS_OK (0x0000) - Success

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid.


Macro Definition Documentation#

SL_CRC_POLYNOMIAL#

#define SL_CRC_POLYNOMIAL
Value:
0x04C11DB7

Polynomial used for CRC calculation.


SL_CRC_POLY_WIDTH#

#define SL_CRC_POLY_WIDTH
Value:
31

Width of the polynomial.


SL_CRC_LFSR_VAL#

#define SL_CRC_LFSR_VAL
Value:
0x0000

Initial LFSR value.


SL_CRC_WIDTH_TYPE#

#define SL_CRC_WIDTH_TYPE
Value:
0

Width type of the CRC.


SL_CRC_DIN_WIDTH#

#define SL_CRC_DIN_WIDTH
Value:
31

Width of the input data.


SL_CRC_NUM_BYTES#

#define SL_CRC_NUM_BYTES
Value:
3

Number of bytes to be written to the CRC.


SL_CRC_AEMPTY#

#define SL_CRC_AEMPTY
Value:
6

Almost empty threshold level.


SL_CRC_AFULL#

#define SL_CRC_AFULL
Value:
2

Almost full threshold level.


SL_CRC_SWAP_DIN#

#define SL_CRC_SWAP_DIN
Value:
0

Whether to swap the input data.


SL_CRC_USE_UDMA#

#define SL_CRC_USE_UDMA
Value:
1

Whether to use uDMA for CRC calculation.


SL_CRC_SWAP_LFSR#

#define SL_CRC_SWAP_LFSR
Value:
1

Whether to swap the LFSR value.