ERROR CODES#
Overview#
Status Codes contains error and status code definitions used by GSDK software components and stacks. This module also provides routines to read the string linked with the error and status codes.
The WiSeConnectâ„¢ SDK v3.x uses Silicon Labs standard status codes. See the Simplicity SDK(formerly Gecko SDK) Status Codes section for more details.
The following section provides a reference to additional status codes returned by the application programming interface (API) that are not included in the list of Silicon Labs standard status codes.