Ultra Low-Power Timer#

Introduction#

Ultra-Low-Power (ULP) timers typically used to operate with extremely low power consumption. These timers are commonly found in battery-powered or energy-efficient devices where minimizing power usage is crucial to extending battery life.

ULP timers typically provide configurable settings, allowing developers to adjust parameters such as clock frequency, timer resolution, and interrupt behavior to meet the specific needs of their applications.

  • The ULP-Timer module supports 4 different instances ulp_timer_instance_t.

  • Each of the ULP-timers can be independently programmed to work in periodic or one-shot mode ulp_timer_mode_t.

  • Each of the ULP-timers can be independently configured as a 32-bit counter or as a microsecond timer ulp_timer_type_t.

Configuration#

  • For more information on configuring available parameters refer to the respective peripheral example readme document.

Usage#

The common ULP-timer functions can be used after ulp-timer Structures are specified, passing an instance of ulp_timer_config_t.

  • These functions will initiate and configure the ULP-timer below, which is the flow for implementation.

  1. sl_si91x_ulp_timer_init

  2. sl_si91x_ulp_timer_set_configuration

  3. sl_si91x_ulp_timer_register_timeout_callback

  4. sl_si91x_ulp_timer_start

  5. sl_si91x_ulp_timer_stop

  6. sl_si91x_ulp_timer_deinit

  • Above functions allow for initializing the ULP-TIMER instance and generates interrupt upon expiration.

  • Below section shows functions to read timer parameters:

  1. sl_si91x_ulp_timer_get_mode

  2. sl_si91x_ulp_timer_get_type

  3. sl_si91x_ulp_timer_get_direction

  4. sl_si91x_ulp_timer_get_count

Modules#

ulp_timer_clk_src_config_t

ulp_timer_config_t

sl_ulp_timer_version_t

Enumerations#

enum
ULP_TIMER_0
ULP_TIMER_1
ULP_TIMER_2
ULP_TIMER_3
ULP_TIMER_LAST
}

Enumeration to represent ULP-timer instances.

enum
ULP_TIMER_MODE_ONESHOT
ULP_TIMER_MODE_PERIODIC
ULP_TIMER_MODE_LAST
}

Enumeration to represent ULP-timer modes.

enum
ULP_TIMER_TYP_DEFAULT
ULP_TIMER_TYP_1US
ULP_TIMER_TYP_256US
ULP_TIMER_TYP_LAST
}

Enumeration to represent ULP-timer types.

enum
ULP_TIMER_REF_CLK_SRC
ULP_TIMER_32KHZ_RO_CLK_SRC
ULP_TIMER_32KHZ_RC_CLK_SRC
ULP_TIMER_32KHZ_XTAL_CLK_SRC
ULP_TIMER_32MHZ_RC_CLK_SRC
ULP_TIMER_20MHZ_RO_CLK_SRC
ULP_TIMER_ULP_CLK_SRC_LAST
}

Enumeration to represent values of clock sources to select as Timer clock.

Typedefs#

typedef void(*

Typedef for the function pointer of the callback function.

typedef CLK_ENABLE_T

Renaming clock type enum.

typedef ulp_timer_dir_t

Renaming clock type enum.

Variables#

uint8_t

true to enable static and false to enable dynamic clock type

boolean_t

true to enable and false to disable ULP timer in synchronous mode to ULPSS pclk

uint8_t

timer input clock source, refer ulp_timer_clk_input_source_t for possible values

boolean_t

true to wait and false to Skip waiting for switching timer clk

uint8_t

timer number, SL_ULP_TIMER_NUMBER for default values

uint8_t

timer mode, SL_ULP_TIMER_MODE for default values

uint8_t

timer type, SL_ULP_TIMER_TYPE for default values

uint32_t

timer match value SL_ULP_TIMER_MATCH_VALUE(delay time) in microseconds

uint8_t

timer direction, SL_ULP_TIMER_DIRECTION for default values

uint8_t

Release version number.

uint8_t

sqa version number

uint8_t

dev version number

Functions#

sl_status_t
sl_si91x_ulp_timer_init(ulp_timer_clk_src_config_t *timer_clk_ptr)

This API will initialize the ULP-Timer by enabling its clock source.

sl_status_t
sl_si91x_ulp_timer_configure_clock(ulp_timer_clk_src_config_t *timer_clk_ptr)

This API will configures and enables the ULP-Timer input clock source.

sl_status_t
sl_si91x_ulp_timer_set_configuration(ulp_timer_config_t *timer_config_ptr)

This API will configure the ULP-Timer parameters.

sl_status_t
sl_si91x_ulp_timer_start(ulp_timer_instance_t timer_num)

This API will start the ULP-Timer.

sl_status_t
sl_si91x_ulp_timer_stop(ulp_timer_instance_t timer_num)

This API will stop the 'timer_num' instance of timer.

sl_status_t
sl_si91x_ulp_timer_restart(ulp_timer_instance_t timer_num)

This API will restart an already running ULP-Timer.

sl_status_t
sl_si91x_ulp_timer_set_type(ulp_timer_instance_t timer_num, ulp_timer_type_t timer_type)

This API will set the ULP-Timer type.

sl_status_t
sl_si91x_ulp_timer_set_direction(ulp_timer_instance_t timer_num, ulp_timer_direction_t timer_direction)

This API will set the ULP-Timer direction.

sl_status_t
sl_si91x_ulp_timer_set_mode(ulp_timer_instance_t timer_num, ulp_timer_mode_t timer_mode)

This API will set the ULP-Timer Mode as one-shot or periodic.

sl_status_t
sl_si91x_ulp_timer_set_count(ulp_timer_instance_t timer_num, uint32_t timer_match_value)

This API will sets the ULP-Timer match value.

sl_status_t
sl_si91x_ulp_timer_get_count(ulp_timer_instance_t timer_num, uint32_t *count_value)

This API will read the ULP-Timer current count.

sl_status_t
sl_si91x_ulp_timer_get_type(ulp_timer_instance_t timer_num, uint32_t *timer_type)

This API will read the ULP-Timer type.

sl_status_t
sl_si91x_ulp_timer_get_mode(ulp_timer_instance_t timer_num, uint32_t *timer_mode)

This API will reads the ULP-Timer mode.

sl_status_t
sl_si91x_ulp_timer_get_direction(ulp_timer_instance_t timer_num, uint32_t *timer_direction)

This API will read the ULP-Timer direction (up-counter or down-counter).

sl_status_t
sl_si91x_ulp_timer_register_timeout_callback(ulp_timer_instance_t timer_num, ulp_timer_callback_t on_timeout_callback)

This API will registers the callback for the timer timeout interrupt and enables the interrupt, as per instance.

sl_status_t
sl_si91x_ulp_timer_unregister_timeout_callback(ulp_timer_instance_t timer_num)

This API will unregister the callback for the timer interrupt and disabling its interrupts as per timer instance.

sl_status_t
sl_si91x_ulp_timer_configure_soc_clock(boolean_t div_factor_type, uint16_t div_factor)

This API will configure the ULPSS SOC clock from M4 SOC clock, to enable the SOC clock source.

sl_status_t

This API will configure the XTAL clock, when clock source is external XTAL clock.

void

This API will de-Initializes the ULP-Timer clock by disabling the peripheral clock.

This API will get the ULP-timer API version.

Macros#

#define

default 1-second timer match-value for down-counter timer-type with 20Mhz clock

Enumeration Documentation#

ulp_timer_instance_t#

ulp_timer_instance_t

Enumeration to represent ULP-timer instances.

Enumerator
ULP_TIMER_0

ULP Timer0 Instance.

ULP_TIMER_1

ULP Timer1 Instance.

ULP_TIMER_2

ULP Timer2 Instance.

ULP_TIMER_3

ULP Timer3 Instance.

ULP_TIMER_LAST

Last member of enum for validation.


ulp_timer_mode_t#

ulp_timer_mode_t

Enumeration to represent ULP-timer modes.

Enumerator
ULP_TIMER_MODE_ONESHOT

ULP Timer one-shot mode.

ULP_TIMER_MODE_PERIODIC

ULP Timer periodic mode.

ULP_TIMER_MODE_LAST

Last member of enum for validation.


ulp_timer_type_t#

ulp_timer_type_t

Enumeration to represent ULP-timer types.

Enumerator
ULP_TIMER_TYP_DEFAULT

ULP Timer normal down counter type.

ULP_TIMER_TYP_1US

ULP Timer one microsecond type.

ULP_TIMER_TYP_256US

ULP Timer 256 microsecond type.

ULP_TIMER_TYP_LAST

Last member of enum for validation.


ulp_timer_clk_input_source_t#

ulp_timer_clk_input_source_t

Enumeration to represent values of clock sources to select as Timer clock.

Enumerator
ULP_TIMER_REF_CLK_SRC

ref clock input source

ULP_TIMER_32KHZ_RO_CLK_SRC

32 kHz ro clock input source

ULP_TIMER_32KHZ_RC_CLK_SRC

32 kHz rc clock input source

ULP_TIMER_32KHZ_XTAL_CLK_SRC

32 kHz xtal clock input source

ULP_TIMER_32MHZ_RC_CLK_SRC

32 MHz rc clock input source

ULP_TIMER_20MHZ_RO_CLK_SRC

20 MHz ro clock input source

ULP_TIMER_ULP_CLK_SRC_LAST

Last member of enum for validation.


Typedef Documentation#

ulp_timer_callback_t#

typedef void(* ulp_timer_callback_t) (void) )(void)

Typedef for the function pointer of the callback function.


ulp_timer_clock_t#

typedef CLK_ENABLE_T ulp_timer_clock_t

Renaming clock type enum.


ulp_timer_direction_t#

typedef ulp_timer_dir_t ulp_timer_direction_t

Renaming clock type enum.


Variable Documentation#

ulp_timer_clk_type#

uint8_t ulp_timer_clk_src_config_t::ulp_timer_clk_type

true to enable static and false to enable dynamic clock type


ulp_timer_sync_to_ulpss_pclk#

boolean_t ulp_timer_clk_src_config_t::ulp_timer_sync_to_ulpss_pclk

true to enable and false to disable ULP timer in synchronous mode to ULPSS pclk


ulp_timer_clk_input_src#

uint8_t ulp_timer_clk_src_config_t::ulp_timer_clk_input_src

timer input clock source, refer ulp_timer_clk_input_source_t for possible values


ulp_timer_skip_switch_time#

boolean_t ulp_timer_clk_src_config_t::ulp_timer_skip_switch_time

true to wait and false to Skip waiting for switching timer clk


timer_num#

uint8_t ulp_timer_config_t::timer_num

timer number, SL_ULP_TIMER_NUMBER for default values


timer_mode#

uint8_t ulp_timer_config_t::timer_mode

timer mode, SL_ULP_TIMER_MODE for default values


timer_type#

uint8_t ulp_timer_config_t::timer_type

timer type, SL_ULP_TIMER_TYPE for default values


timer_match_value#

uint32_t ulp_timer_config_t::timer_match_value

timer match value SL_ULP_TIMER_MATCH_VALUE(delay time) in microseconds


timer_direction#

uint8_t ulp_timer_config_t::timer_direction

timer direction, SL_ULP_TIMER_DIRECTION for default values


release#

uint8_t sl_ulp_timer_version_t::release

Release version number.


major#

uint8_t sl_ulp_timer_version_t::major

sqa version number


minor#

uint8_t sl_ulp_timer_version_t::minor

dev version number


Function Documentation#

sl_si91x_ulp_timer_init#

sl_status_t sl_si91x_ulp_timer_init (ulp_timer_clk_src_config_t * timer_clk_ptr)

This API will initialize the ULP-Timer by enabling its clock source.

Parameters
TypeDirectionArgument NameDescription
ulp_timer_clk_src_config_t *[in]timer_clk_ptr

Pointer to timer_clk configuration structure

It configures clock frequency, clock-type, enables/disables synchronization to ULPSS pclk & skips/allows waiting for timer clock switching.

Returns

  • status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Timer clock type or timer clock source values are invalid

    • SL_STATUS_INVALID_CONFIGURATION (0x0023) - Timer clock-source configuration structure members have invalid configurations.

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer

    • SL_STATUS_OK (0x0000) - Success, timer clock-source parameters configured properly


sl_si91x_ulp_timer_configure_clock#

sl_status_t sl_si91x_ulp_timer_configure_clock (ulp_timer_clk_src_config_t * timer_clk_ptr)

This API will configures and enables the ULP-Timer input clock source.

Parameters
TypeDirectionArgument NameDescription
ulp_timer_clk_src_config_t *[in]timer_clk_ptr

Pointer to timer_clk configuration structure ulp_timer_clk_src_config_t.

It configures clock frequency, clock-type, enables/disables synchronization to ULPSS pclk & skips/allows waiting for timer clock switching. It is called inside sl_si91x_ulp_timer_init API.

Note

Returns

  • status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Timer clock type or timer clock source values are invalid

    • SL_STATUS_INVALID_CONFIGURATION (0x0023) - Timer clock-source configuration structure members have invalid configurations.

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer

    • SL_STATUS_OK (0x0000) - Success, timer clock-source parameters configured properly


sl_si91x_ulp_timer_set_configuration#

sl_status_t sl_si91x_ulp_timer_set_configuration (ulp_timer_config_t * timer_config_ptr)

This API will configure the ULP-Timer parameters.

Parameters
TypeDirectionArgument NameDescription
ulp_timer_config_t *[in]timer_config_ptr

Pointer to the timer_configuration structure ulp_timer_config_t.

It configures the parameters such as timer number, mode, type, match-value, and direction. Also configures the integral and fractional values of clock cycles per microseconds or per 256 microseconds as per the selected timer-type.

Returns

  • status 0 if successful, else error code as follows:

    • SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer

    • SL_STATUS_INVALID_INDEX (0x0027) - Timer configuration structure member 'timer_num' has an invalid value.

    • SL_STATUS_INVALID_MODE (0x0024) - Timer configuration structure member 'timer_mode' has an invalid value.

    • SL_STATUS_INVALID_TYPE (0x0026) - Timer configuration structure member 'timer_type' has an invalid value.

    • SL_STATUS_INVALID_PARAMETER (0x0021) - Timer configuration structure member 'timer_direction' has an invalid value.

    • SL_STATUS_OK (0x0000) - Success, timer parameters are configured properly


sl_si91x_ulp_timer_start#

sl_status_t sl_si91x_ulp_timer_start (ulp_timer_instance_t timer_num)

This API will start the ULP-Timer.

Parameters
TypeDirectionArgument NameDescription
ulp_timer_instance_t[in]timer_num

enum for ULP-timer Number (0 to 3), ulp_timer_instance_t for possible values

Note

  • Timer instance must not be in running state when calling this API.

Returns

  • status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_INDEX (0x0027) - 'timer_num' parameter value is invalid.

    • SL_STATUS_OK (0x0000) - Successfully started the timer instance


sl_si91x_ulp_timer_stop#

sl_status_t sl_si91x_ulp_timer_stop (ulp_timer_instance_t timer_num)

This API will stop the 'timer_num' instance of timer.

Parameters
TypeDirectionArgument NameDescription
ulp_timer_instance_t[in]timer_num

enum for ULP-timer Number (0 to 3), ulp_timer_instance_t for possible values

Sets the stop bit of timer control register, which is a self clearing bit. This will only stops the timer but not disables it. To disable it use sl_si91x_ulp_timer_deinit.

Returns

  • status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_INDEX (0x0027) - 'timer_num' parameter value is invalid.

    • SL_STATUS_OK (0x0000) - Successfully stopped the timer instance


sl_si91x_ulp_timer_restart#

sl_status_t sl_si91x_ulp_timer_restart (ulp_timer_instance_t timer_num)

This API will restart an already running ULP-Timer.

Parameters
TypeDirectionArgument NameDescription
ulp_timer_instance_t[in]timer_num

enum for ULP-timer Number, ulp_timer_instance_t for possible values

ULP-Timer restart which means it will first stop the timer instance and then starts it again. This will just restart the currently running counter.

Returns

  • status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_INDEX (0x0027) - 'timer_num' parameter value is invalid.

    • SL_STATUS_OK (0x0000) - Successfully restarted the timer instance


sl_si91x_ulp_timer_set_type#

sl_status_t sl_si91x_ulp_timer_set_type (ulp_timer_instance_t timer_num, ulp_timer_type_t timer_type)

This API will set the ULP-Timer type.

Parameters
TypeDirectionArgument NameDescription
ulp_timer_instance_t[in]timer_num

enum for ULP-timer Number, ulp_timer_instance_t for possible values

ulp_timer_type_t[in]timer_type

enum for ULP-timer Type, ulp_timer_type_t for possible values

Timer types include 256 µs, 1 µs, and count-down.

  • 1 microsecond type : The time unit is 1µs.

  • 256 microsecond type : The time unit is 256µs.

  • Count-down timer type : The time unit is one clock cycle period. Note

    • This API should be used when timer is stopped.

    Returns

    • status 0 if successful, else error code as follows:

      • SL_STATUS_INVALID_INDEX (0x0027) - 'timer_num' parameter value is invalid.

      • SL_STATUS_INVALID_TYPE (0x0026) - 'timer_type' parameter value is invalid.

      • SL_STATUS_OK (0x0000) - Successfully set timer-type


sl_si91x_ulp_timer_set_direction#

sl_status_t sl_si91x_ulp_timer_set_direction (ulp_timer_instance_t timer_num, ulp_timer_direction_t timer_direction)

This API will set the ULP-Timer direction.

Parameters
TypeDirectionArgument NameDescription
ulp_timer_instance_t[in]timer_num

enum for ULP-timer Number, ulp_timer_instance_t for possible values

ulp_timer_direction_t[in]timer_direction

enum for ULP-timer direction, ulp_timer_direction_t for possible values

ULP timer set direction will set the ULP-Timer direction as up-counting or down-counting, by default it works as down-counter. Note

  • This API should be used when timer is stopped.

Returns

  • status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_INDEX (0x0027) - 'timer_num' parameter value is invalid.

    • SL_STATUS_INVALID_PARAMETER (0x0021) - 'timer_direction' parameter value is invalid.

    • SL_STATUS_OK (0x0000) - Successfully set timer-direction


sl_si91x_ulp_timer_set_mode#

sl_status_t sl_si91x_ulp_timer_set_mode (ulp_timer_instance_t timer_num, ulp_timer_mode_t timer_mode)

This API will set the ULP-Timer Mode as one-shot or periodic.

Parameters
TypeDirectionArgument NameDescription
ulp_timer_instance_t[in]timer_num

enum for ULP-timer Number, ulp_timer_instance_t for possible values

ulp_timer_mode_t[in]timer_mode

enum for ULP-timer mode, ulp_timer_mode_t for possible values

In one shot operation, the timer counts till the timeout and then generates a single interrupt after which it returns to idle state. Where as in periodic operation the timer generates interrupts continously with interval equal to timeout. This API should be used when timer is stopped

Returns

  • status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_INDEX (0x0027) - 'timer_num' parameter value is invalid.

    • SL_STATUS_INVALID_MODE (0x0024) - 'timer_mode' parameter value is invalid.

    • SL_STATUS_OK (0x0000) - Successfully set timer-mode


sl_si91x_ulp_timer_set_count#

sl_status_t sl_si91x_ulp_timer_set_count (ulp_timer_instance_t timer_num, uint32_t timer_match_value)

This API will sets the ULP-Timer match value.

Parameters
TypeDirectionArgument NameDescription
ulp_timer_instance_t[in]timer_num

enum for ULP-timer Number, ulp_timer_instance_t for possible values.

uint32_t[in]timer_match_value

for ULP-timer timeout value

When the timer reaches the match value & if the interrupt is enabled it will generate an interrupt to the processor.

  • For one microsecond type, match-value = number of microseconds

  • For 256 microsecond type, match-value = (time in microseconds)/256

  • For normal up/down counter type, timer = (number of clock cycles per microseconds * time in microseconds).

Note

  • This API should be used when timer is stopped.

Returns

  • status 0 if successful, else error-code

    • SL_STATUS_INVALID_INDEX (0x0027) - 'timer_num' parameter value is invalid.

    • SL_STATUS_OK (0x0000) - Successfully set timer match value.


sl_si91x_ulp_timer_get_count#

sl_status_t sl_si91x_ulp_timer_get_count (ulp_timer_instance_t timer_num, uint32_t * count_value)

This API will read the ULP-Timer current count.

Parameters
TypeDirectionArgument NameDescription
ulp_timer_instance_t[in]timer_num

enum for ULP-timer Number, ulp_timer_instance_t for possible values.

uint32_t *[in]count_value

Pointer to variable which will store the current count of the timer

If counter-down is set then counter register bits indicate time remaining before timeout (read as 32'hFFFF_FFFF initially). If counter-up is set then these bits directly gives out the up-running counter/timer value. Updates the timer current-count value to the count-value variable, passed as reference by user (2nd argument).

Returns

  • status 0 if successful, else error code as follows:

    • SL_STATUS_NULL_POINTER (0x0022) - 'Pointer to count_value' parameter is a null pointer.

    • SL_STATUS_INVALID_INDEX (0x0027) - 'timer_num' parameter value is invalid.

    • SL_STATUS_OK (0x0000) - Successfully read the timer's current count value


sl_si91x_ulp_timer_get_type#

sl_status_t sl_si91x_ulp_timer_get_type (ulp_timer_instance_t timer_num, uint32_t * timer_type)

This API will read the ULP-Timer type.

Parameters
TypeDirectionArgument NameDescription
ulp_timer_instance_t[in]timer_num

enum for ULP-timer Number, ulp_timer_instance_t for possible values.

uint32_t *[in]timer_type

Pointer to variable which will store the current type of the timer

Updates the timer type value to the timer_type variable, passed as reference by user.

  • '0' for down-counter type

  • '1' for 1us type

  • '2' for 256us type

Returns

  • status 0 if successful, else error code as follows:

    • SL_STATUS_NULL_POINTER (0x0022) - 'Pointer to timer_type' parameter is a null pointer.

    • SL_STATUS_INVALID_INDEX (0x0027) - 'timer_num' parameter value is invalid.

    • SL_STATUS_OK (0x0000) - Successfully read the timer's current type


sl_si91x_ulp_timer_get_mode#

sl_status_t sl_si91x_ulp_timer_get_mode (ulp_timer_instance_t timer_num, uint32_t * timer_mode)

This API will reads the ULP-Timer mode.

Parameters
TypeDirectionArgument NameDescription
ulp_timer_instance_t[in]timer_num

enum for ULP-timer Number, ulp_timer_instance_t for possible values.

uint32_t *[in]timer_mode

Pointer to variable which will store the current mode of the timer

Updates the timer mode value to the timer_mode variable, passed as reference by user.

  • '0' for one-shot mode

  • '1' for periodic mode

Returns

  • status 0 if successful, else error code as follows:

    • SL_STATUS_NULL_POINTER (0x0022) - 'Pointer to timer_mode' parameter is a null pointer.

    • SL_STATUS_INVALID_INDEX (0x0027) - 'timer_num' parameter value is invalid.

    • SL_STATUS_OK (0x0000) - Successfully read the timer's current mode


sl_si91x_ulp_timer_get_direction#

sl_status_t sl_si91x_ulp_timer_get_direction (ulp_timer_instance_t timer_num, uint32_t * timer_direction)

This API will read the ULP-Timer direction (up-counter or down-counter).

Parameters
TypeDirectionArgument NameDescription
ulp_timer_instance_t[in]timer_num

enum for ULP-timer Number, ulp_timer_instance_t for possible values.

uint32_t *[in]timer_direction

Pointer to variable which will store the current direction of the timer

Updates the timer direction to the timer_direction variable, passed as reference by user.

  • '0' for down-counting

  • '1' for up-counting

Returns

  • status 0 if successful, else error code as follows:

    • SL_STATUS_NULL_POINTER (0x0022) - 'Pointer to timer_direction' parameter is a null pointer.

    • SL_STATUS_INVALID_INDEX (0x0027) - 'timer_num' parameter value is invalid.

    • SL_STATUS_OK (0x0000) - Successfully read the timer's current direction


sl_si91x_ulp_timer_register_timeout_callback#

sl_status_t sl_si91x_ulp_timer_register_timeout_callback (ulp_timer_instance_t timer_num, ulp_timer_callback_t on_timeout_callback)

This API will registers the callback for the timer timeout interrupt and enables the interrupt, as per instance.

Parameters
TypeDirectionArgument NameDescription
ulp_timer_instance_t[in]timer_num

enum for ULP-timer Number, ulp_timer_instance_t for possible values.

ulp_timer_callback_t[in]on_timeout_callback

(function pointer) Callback function pointer to be called when the timer timeout interrupt occurred.

If any callback is already registered, the user needs to unregister the callback first before registering the callback else it will return call SL_STATUS_BUSY error.

Returns

  • status 0 if successful, else error code as follows:

    • SL_STATUS_NULL_POINTER (0x0022) - 'pointer to callback_data_input' parameter is a null pointer.

    • SL_STATUS_INVALID_INDEX (0x0027) - 'timer_num' parameter value is invalid.

    • SL_STATUS_ALLOCATION_FAILED (0x0019) - Timer interrupt enabling failed.

    • SL_STATUS_BUSY (0x0004) - The callback is already registered, unregister the previous callback before registering a new one.

    • SL_STATUS_OK (0x0000) - Successfully registered the timer timeout callback


sl_si91x_ulp_timer_unregister_timeout_callback#

sl_status_t sl_si91x_ulp_timer_unregister_timeout_callback (ulp_timer_instance_t timer_num)

This API will unregister the callback for the timer interrupt and disabling its interrupts as per timer instance.

Parameters
TypeDirectionArgument NameDescription
ulp_timer_instance_t[in]timer_num

enum for ULP-timer Number, ulp_timer_instance_t for possible values.

Returns

  • status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_INDEX (0x0027) - 'timer_num' parameter value is invalid.

    • SL_STATUS_ALLOCATION_FAILED (0x0019) - Timer interrupt disabling failed.

    • SL_STATUS_OK (0x0000) - Successfully unregistered the timer timeout callback


sl_si91x_ulp_timer_configure_soc_clock#

sl_status_t sl_si91x_ulp_timer_configure_soc_clock (boolean_t div_factor_type, uint16_t div_factor)

This API will configure the ULPSS SOC clock from M4 SOC clock, to enable the SOC clock source.

Parameters
TypeDirectionArgument NameDescription
boolean_t[in]div_factor_type

value to divide the clock, ensure that it should be an odd number if div_factor_type is 1 & vice versa

uint16_t[in]div_factor

selects the type of divider for m4_soc_clk_2ulpss

  • '0' Even Divider is selected

  • '1' Odd Divider is selected

This API is used to select the ULPSS processor clock source as timer input clock source which is greater than 100MHz(used for high-power mode) To divide the clock, ensure that it should be odd number if div_factor_type is 1 & viceversa Div_factor_type selects the type of divider for m4_soc_clk_2ulpss

  • '0' Even Divider is selected

  • '1' Odd Divider is selected Use this API in place of timer clock config API, when using SOC clock source with timer in high power mode

Returns

  • status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER(0x0021) - 'div_factor' is not according to div_factor_type


sl_si91x_ulp_timer_configure_xtal_clock#

sl_status_t sl_si91x_ulp_timer_configure_xtal_clock (uint8_t xtal_pin)

This API will configure the XTAL clock, when clock source is external XTAL clock.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]xtal_pin

: Pin number of NPSS_GPIO. Possible values are 0 to 4.

To enable the external XTAL clk source need to call this API before calling sl_si91x_ulp_timer_configure_clock API.

Returns

  • status 0 if successful, else error code as follows:

    • SL_STATUS_INVALID_PARAMETER(0x0021) - 'xtal_pin' parameter value is invalid.


sl_si91x_ulp_timer_deinit#

void sl_si91x_ulp_timer_deinit (void )

This API will de-Initializes the ULP-Timer clock by disabling the peripheral clock.

Parameters
TypeDirectionArgument NameDescription
voidN/A

It also Unregisters callback of all timer instances

Returns

  • none

Note

  • Unregisters the callbacks of all timer instances


sl_si91x_ulp_timer_get_version#

sl_ulp_timer_version_t sl_si91x_ulp_timer_get_version (void )

This API will get the ULP-timer API version.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This API is used to know the API version of ULP_TIMER.

Returns


Macro Definition Documentation#

SL_TIMER_MATCH_VALUE_DEFAULT#

#define SL_TIMER_MATCH_VALUE_DEFAULT
Value:
  20000000

default 1-second timer match-value for down-counter timer-type with 20Mhz clock


SL_ULP_TIMER_CLK_TYPE_STATIC#

#define SL_ULP_TIMER_CLK_TYPE_STATIC
Value:
1

SL_ULP_TIMER_CLK_TYPE_DYNAMIC#

#define SL_ULP_TIMER_CLK_TYPE_DYNAMIC
Value:
0