Structure to hold the parameters of timer clock-source configurations.
Public Attributes#
uint8_t
true to enable static and false to enable dynamic clock type
boolean_t
true to enable and false to disable ULP timer in synchronous mode to ULPSS pclk
uint8_t
timer input clock source, refer ulp_timer_clk_input_source_t for possible values
boolean_t
true to wait and false to Skip waiting for switching timer clk
Public Attribute Documentation#
ulp_timer_clk_type#
uint8_t ulp_timer_clk_src_config_t::ulp_timer_clk_type
true to enable static and false to enable dynamic clock type
ulp_timer_sync_to_ulpss_pclk#
boolean_t ulp_timer_clk_src_config_t::ulp_timer_sync_to_ulpss_pclk
true to enable and false to disable ULP timer in synchronous mode to ULPSS pclk
ulp_timer_clk_input_src#
uint8_t ulp_timer_clk_src_config_t::ulp_timer_clk_input_src
timer input clock source, refer ulp_timer_clk_input_source_t for possible values
ulp_timer_skip_switch_time#
boolean_t ulp_timer_clk_src_config_t::ulp_timer_skip_switch_time
true to wait and false to Skip waiting for switching timer clk