HTTP client credentials.

Public Attributes#

uint16_t

Length of username. Maximum supported length of username is 139 bytes.

uint16_t

Length of password. Maximum supported length of password is 139 bytes.

uint8_t

A flexible array to store both username and password.

Public Attribute Documentation#

username_length#

uint16_t sl_http_client_credentials_t::username_length

Length of username. Maximum supported length of username is 139 bytes.


Definition at line 128 of file components/service/http_client/inc/sl_http_client.h

password_length#

uint16_t sl_http_client_credentials_t::password_length

Length of password. Maximum supported length of password is 139 bytes.


Definition at line 129 of file components/service/http_client/inc/sl_http_client.h

data#

uint8_t sl_http_client_credentials_t::data[]

A flexible array to store both username and password.


Definition at line 130 of file components/service/http_client/inc/sl_http_client.h