Structure to hold the fifo threshold configuration parameters.
Public Attributes#
uint8_t
Number of channel enable.
uint8_t
AEMPTY Threshold.
uint8_t
AFULL Threshold.
uint8_t
Internal or External DMA.
Public Attribute Documentation#
num_of_channel_en#
uint8_t sl_adc_fifo_thrld_config_t::num_of_channel_en
Number of channel enable.
Definition at line
125
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_adc.h
a_empty_threshold#
uint8_t sl_adc_fifo_thrld_config_t::a_empty_threshold
AEMPTY Threshold.
Definition at line
126
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_adc.h
a_full_threshold#
uint8_t sl_adc_fifo_thrld_config_t::a_full_threshold
AFULL Threshold.
Definition at line
127
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_adc.h
dma_type#
uint8_t sl_adc_fifo_thrld_config_t::dma_type
Internal or External DMA.
Definition at line
128
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_adc.h