Structure to hold the threshold detection configuration parameters.
Public Attributes#
uint16_t
Threshold_1.
uint16_t
Threshold_2.
uint8_t *
Threshold_1 condition like Equal, Grater, Lesser.
uint8_t *
Threshold_2 condition like Equal, Grater, Lesser.
uint8_t
Public Attribute Documentation#
threshold1#
uint16_t sl_adc_threshold_config_t::threshold1
Threshold_1.
Definition at line
116
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_adc.h
threshold2#
uint16_t sl_adc_threshold_config_t::threshold2
Threshold_2.
Definition at line
117
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_adc.h
threshold1_cond#
uint8_t* sl_adc_threshold_config_t::threshold1_cond
Threshold_1 condition like Equal, Grater, Lesser.
Definition at line
118
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_adc.h
threshold2_cond#
uint8_t* sl_adc_threshold_config_t::threshold2_cond
Threshold_2 condition like Equal, Grater, Lesser.
Definition at line
119
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_adc.h
range#
uint8_t sl_adc_threshold_config_t::range
Definition at line
120
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_adc.h