Structure to hold the parameters of timer configurations.
Public Attributes#
CT mode, sl_config_timer_mode_t for its values.
counter-0 soft reset, true to enable & false to disable it
counter-0 periodic mode, true to enable & false to disable it
counter-0 software trigger, true to enable & false to disable it
counter-0 sync trigger, true to enable & false to disable it
counter-0 buffer, true to enable & false to disable it
counter-1 soft reset, true to enable & false to disable it
counter-1 periodic mode, true to enable & false to disable it
counter-1 software trigger, true to enable & false to disable it
counter-1 sync trigger, true to enable & false to disable it
counter-1 buffer, true to enable & false to disable it
counter-0 direction sl_config_timer_counter0_direction_t for possible values
counter-1 direction sl_config_timer_counter1_direction_t for possible values
Public Attribute Documentation#
is_counter_mode_32bit_enabled#
boolean_t sl_config_timer_config_t::is_counter_mode_32bit_enabled
CT mode, sl_config_timer_mode_t for its values.
209
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h
is_counter0_soft_reset_enabled#
boolean_t sl_config_timer_config_t::is_counter0_soft_reset_enabled
counter-0 soft reset, true to enable & false to disable it
210
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h
is_counter0_periodic_enabled#
boolean_t sl_config_timer_config_t::is_counter0_periodic_enabled
counter-0 periodic mode, true to enable & false to disable it
211
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h
is_counter0_trigger_enabled#
boolean_t sl_config_timer_config_t::is_counter0_trigger_enabled
counter-0 software trigger, true to enable & false to disable it
212
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h
is_counter0_sync_trigger_enabled#
boolean_t sl_config_timer_config_t::is_counter0_sync_trigger_enabled
counter-0 sync trigger, true to enable & false to disable it
213
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h
is_counter0_buffer_enabled#
boolean_t sl_config_timer_config_t::is_counter0_buffer_enabled
counter-0 buffer, true to enable & false to disable it
214
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h
is_counter1_soft_reset_enabled#
boolean_t sl_config_timer_config_t::is_counter1_soft_reset_enabled
counter-1 soft reset, true to enable & false to disable it
215
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h
is_counter1_periodic_enabled#
boolean_t sl_config_timer_config_t::is_counter1_periodic_enabled
counter-1 periodic mode, true to enable & false to disable it
216
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h
is_counter1_trigger_enabled#
boolean_t sl_config_timer_config_t::is_counter1_trigger_enabled
counter-1 software trigger, true to enable & false to disable it
217
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h
is_counter1_sync_trigger_enabled#
boolean_t sl_config_timer_config_t::is_counter1_sync_trigger_enabled
counter-1 sync trigger, true to enable & false to disable it
218
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h
is_counter1_buffer_enabled#
boolean_t sl_config_timer_config_t::is_counter1_buffer_enabled
counter-1 buffer, true to enable & false to disable it
219
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h
counter0_direction#
uint8_t sl_config_timer_config_t::counter0_direction
counter-0 direction sl_config_timer_counter0_direction_t for possible values
220
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h
counter1_direction#
uint8_t sl_config_timer_config_t::counter1_direction
counter-1 direction sl_config_timer_counter1_direction_t for possible values
221
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h