Structure to hold various interrupt flags of config-timer.
Public Attributes#
true to enable counter-0 interrupt on event occurrence, false to disable it
true to enable counter-0 interrupt on FIFO full, false to disable it
true to enable counter-0 interrupt on zero count value, false to disable it
true to enable counter-0 interrupt on match-value, false to disable it
true to enable counter-1 interrupt on event occurrence, false to disable it
true to enable counter-1 interrupt on FIFO full, false to disable it
true to enable counter-1 interrupt on zero count value, false to disable it
true to enable counter-1 interrupt on match-value, false to disable it
Public Attribute Documentation#
is_counter0_event_interrupt_enabled#
boolean_t sl_config_timer_interrupt_flags_t::is_counter0_event_interrupt_enabled
true to enable counter-0 interrupt on event occurrence, false to disable it
268
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h
is_counter0_fifo_full_interrupt_enabled#
boolean_t sl_config_timer_interrupt_flags_t::is_counter0_fifo_full_interrupt_enabled
true to enable counter-0 interrupt on FIFO full, false to disable it
270
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h
is_counter0_hit_zero_interrupt_enabled#
boolean_t sl_config_timer_interrupt_flags_t::is_counter0_hit_zero_interrupt_enabled
true to enable counter-0 interrupt on zero count value, false to disable it
272
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h
is_counter0_hit_peak_interrupt_enabled#
boolean_t sl_config_timer_interrupt_flags_t::is_counter0_hit_peak_interrupt_enabled
true to enable counter-0 interrupt on match-value, false to disable it
274
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h
is_counter1_event_interrupt_enabled#
boolean_t sl_config_timer_interrupt_flags_t::is_counter1_event_interrupt_enabled
true to enable counter-1 interrupt on event occurrence, false to disable it
276
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h
is_counter1_fifo_full_interrupt_enabled#
boolean_t sl_config_timer_interrupt_flags_t::is_counter1_fifo_full_interrupt_enabled
true to enable counter-1 interrupt on FIFO full, false to disable it
278
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h
is_counter1_hit_zero_interrupt_enabled#
boolean_t sl_config_timer_interrupt_flags_t::is_counter1_hit_zero_interrupt_enabled
true to enable counter-1 interrupt on zero count value, false to disable it
280
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h
is_counter1_hit_peak_interrupt_enabled#
boolean_t sl_config_timer_interrupt_flags_t::is_counter1_hit_peak_interrupt_enabled
true to enable counter-1 interrupt on match-value, false to disable it
282
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_config_timer.h