Wi-Fi buffer.

Public Attributes#

sl_slist_node_t

Points to the node of the list of which the buffer is part of.

uint32_t

Indicates the buffer size.

uint8_t

Indicates the buffer type (SL_WIFI_TX_FRAME_BUFFER,SL_WIFI_RX_FRAME_BUFFER,etc..) corresponding to the buffer.

uint8_t

Stores the data (header + payload) to be send to TA.

Public Attribute Documentation#

node#

sl_slist_node_t sl_wifi_buffer_t::node

Points to the node of the list of which the buffer is part of.


Definition at line 28 of file components/protocol/wifi/inc/sl_wifi_host_interface.h

length#

uint32_t sl_wifi_buffer_t::length

Indicates the buffer size.


Definition at line 29 of file components/protocol/wifi/inc/sl_wifi_host_interface.h

type#

uint8_t sl_wifi_buffer_t::type

Indicates the buffer type (SL_WIFI_TX_FRAME_BUFFER,SL_WIFI_RX_FRAME_BUFFER,etc..) corresponding to the buffer.


Definition at line 31 of file components/protocol/wifi/inc/sl_wifi_host_interface.h

data#

uint8_t sl_wifi_buffer_t::data[]

Stores the data (header + payload) to be send to TA.


Definition at line 32 of file components/protocol/wifi/inc/sl_wifi_host_interface.h