Wi-Fi max transmit power.
Note
The effective transmit power is subject to regional and device limitations. If the specified transmit power exceeds the maximum supported value for that region or if the specified transmit power exceeds the maximum supported value of the device, the transmission will occur at the maximum supported transmit power.
Public Attributes#
uint8_t
Transmit power during scan. Valid input range: 1dBm to 31dBm.
uint8_t
Transmit power during join. Valid input range: 1dBm to 31dBm.
Public Attribute Documentation#
scan_tx_power#
uint8_t sl_wifi_max_tx_power_t::scan_tx_power
Transmit power during scan. Valid input range: 1dBm to 31dBm.
Definition at line
456
of file components/protocol/wifi/inc/sl_wifi_types.h
join_tx_power#
uint8_t sl_wifi_max_tx_power_t::join_tx_power
Transmit power during join. Valid input range: 1dBm to 31dBm.
Definition at line
457
of file components/protocol/wifi/inc/sl_wifi_types.h