Wi-Fi transceiver RX Data callback structure.

Public Attributes#

sl_status_t

Status code for the received RX packet.

int8_t

RSSI of the received 802.11 frame. This field is valid only if status is set to success.

uint32_t

Rate of the received 802.11 frame as per sl_wifi_data_rate_t. This field is valid only if status is set to success.

uint32_t

Length of the buffer.

uint8_t *

IEEE 802.11 frame received from firmware.

Public Attribute Documentation#

status#

sl_status_t sl_wifi_transceiver_rx_data_t::status

Status code for the received RX packet.

Status

Description

SL_STATUS_OK (0x0)

Success

SL_STATUS_UNKNOWN_PEER (0x3)

If SL_SI91X_FEAT_TRANSCEIVER_MAC_PEER_DS_SUPPORT feature is enabled and data packet is received from a peer not present in MAC layer


Definition at line 600 of file components/protocol/wifi/inc/sl_wifi_types.h

rssi#

int8_t sl_wifi_transceiver_rx_data_t::rssi

RSSI of the received 802.11 frame. This field is valid only if status is set to success.


Definition at line 602 of file components/protocol/wifi/inc/sl_wifi_types.h

rate#

uint32_t sl_wifi_transceiver_rx_data_t::rate

Rate of the received 802.11 frame as per sl_wifi_data_rate_t. This field is valid only if status is set to success.


Definition at line 604 of file components/protocol/wifi/inc/sl_wifi_types.h

length#

uint32_t sl_wifi_transceiver_rx_data_t::length

Length of the buffer.


Definition at line 606 of file components/protocol/wifi/inc/sl_wifi_types.h

buffer#

uint8_t* sl_wifi_transceiver_rx_data_t::buffer

IEEE 802.11 frame received from firmware.

buffer points to the beginning of the MAC header. Contents are not valid once the function returns. If the contents need to be accessed after return, it needs to be copied to the application buffer. If the status is not successful, buffer is set to NULL and shall not be accessed.

Format of IEEE 802.11 frame received from firmware in buffer

Field name

Frame Control

Duration

Addr1

Addr2

Adddr3

Seq Ctrl

Addr4

QoS ctrl

Payload (LLC + Data)

Size(bytes)

2

2

6

6

6

2

6 (Optionally present)

2 (Optionally present)

Variable

Note

  • All unicast data frames received where Address 1 (RA) matches the device MAC address are passed to the host application.

  • All broadcast data frames are sent to the host.

  • All multicast data frames are sent to the host unless filtering is enabled using sl_wifi_set_transceiver_multicast_filter.

  • On chip duplicate detection is not supported and is expected to be handled by the application.

  • On chip MAC level decryption is not supported.


Definition at line 618 of file components/protocol/wifi/inc/sl_wifi_types.h