Wi-Fi Access Point configuration structure.
Indicates the configuration parameters for setting up a Wi-Fi Access Point (AP).
Public Attributes#
SSID (Service Set Identifier) of the Access Point.
Security mode of the Access Point.
Encryption mode of the Access Point.
Channel configuration of the Access Point.
Rate protocol of the Access Point.
Optional flags for AP configuration.
ID of secure credentials.
Keep alive type of the access point. One of the values from sl_si91x_ap_keepalive_type_t
Beacon interval of the access point in milliseconds.
Duration in milliseconds to kick idle client.
Number of beacons per DTIM.
Maximum number of associated clients.
Flag to stop beaconing when there are no associated clients.
Flags to enable Transition Disable Indication (TDI). One of the values from sl_wifi_tdi_t.
A flag to enable 11n.
Public Attribute Documentation#
ssid#
sl_wifi_ssid_t sl_wifi_ap_configuration_t::ssid
SSID (Service Set Identifier) of the Access Point.
238
of file components/protocol/wifi/inc/sl_wifi_types.h
security#
sl_wifi_security_t sl_wifi_ap_configuration_t::security
Security mode of the Access Point.
239
of file components/protocol/wifi/inc/sl_wifi_types.h
encryption#
sl_wifi_encryption_t sl_wifi_ap_configuration_t::encryption
Encryption mode of the Access Point.
240
of file components/protocol/wifi/inc/sl_wifi_types.h
channel#
sl_wifi_channel_t sl_wifi_ap_configuration_t::channel
Channel configuration of the Access Point.
241
of file components/protocol/wifi/inc/sl_wifi_types.h
rate_protocol#
sl_wifi_rate_protocol_t sl_wifi_ap_configuration_t::rate_protocol
Rate protocol of the Access Point.
242
of file components/protocol/wifi/inc/sl_wifi_types.h
options#
sl_wifi_ap_flag_t sl_wifi_ap_configuration_t::options
Optional flags for AP configuration.
243
of file components/protocol/wifi/inc/sl_wifi_types.h
credential_id#
sl_wifi_credential_id_t sl_wifi_ap_configuration_t::credential_id
ID of secure credentials.
244
of file components/protocol/wifi/inc/sl_wifi_types.h
keepalive_type#
uint8_t sl_wifi_ap_configuration_t::keepalive_type
Keep alive type of the access point. One of the values from sl_si91x_ap_keepalive_type_t
246
of file components/protocol/wifi/inc/sl_wifi_types.h
beacon_interval#
uint16_t sl_wifi_ap_configuration_t::beacon_interval
Beacon interval of the access point in milliseconds.
247
of file components/protocol/wifi/inc/sl_wifi_types.h
client_idle_timeout#
uint32_t sl_wifi_ap_configuration_t::client_idle_timeout
Duration in milliseconds to kick idle client.
248
of file components/protocol/wifi/inc/sl_wifi_types.h
dtim_beacon_count#
uint16_t sl_wifi_ap_configuration_t::dtim_beacon_count
Number of beacons per DTIM.
249
of file components/protocol/wifi/inc/sl_wifi_types.h
maximum_clients#
uint8_t sl_wifi_ap_configuration_t::maximum_clients
Maximum number of associated clients.
250
of file components/protocol/wifi/inc/sl_wifi_types.h
beacon_stop#
uint8_t sl_wifi_ap_configuration_t::beacon_stop
Flag to stop beaconing when there are no associated clients.
251
of file components/protocol/wifi/inc/sl_wifi_types.h
tdi_flags#
sl_wifi_tdi_t sl_wifi_ap_configuration_t::tdi_flags
Flags to enable Transition Disable Indication (TDI). One of the values from sl_wifi_tdi_t.
253
of file components/protocol/wifi/inc/sl_wifi_types.h
is_11n_enabled#
uint8_t sl_wifi_ap_configuration_t::is_11n_enabled
A flag to enable 11n.
254
of file components/protocol/wifi/inc/sl_wifi_types.h