Wi-Fi firmware version information.

Contains the detailed information about the Wi-Fi firmware version.

Public Attributes#

uint8_t

Chip ID.

uint8_t

ROM ID.

uint8_t

Major version number.

uint8_t

Minor version number.

uint8_t

Security enabled or disabled.

uint8_t

Patch number.

uint8_t

Customer ID.

uint16_t

Build number.

Public Attribute Documentation#

chip_id#

uint8_t sl_wifi_firmware_version_t::chip_id

Chip ID.


rom_id#

uint8_t sl_wifi_firmware_version_t::rom_id

ROM ID.


major#

uint8_t sl_wifi_firmware_version_t::major

Major version number.


minor#

uint8_t sl_wifi_firmware_version_t::minor

Minor version number.


security_version#

uint8_t sl_wifi_firmware_version_t::security_version

Security enabled or disabled.


patch_num#

uint8_t sl_wifi_firmware_version_t::patch_num

Patch number.


customer_id#

uint8_t sl_wifi_firmware_version_t::customer_id

Customer ID.


build_num#

uint16_t sl_wifi_firmware_version_t::build_num

Build number.