Wi-Fi transceiver contention window configuration structure.

Specifies the configuration parameters for the contention window of the Wi-Fi transceiver.

Public Attributes#

uint8_t

Minimum contention window size. Value is calculated from 2^N - 1 where exponent shall be provided as the input. Valid values for exponent N are 0 - 15.

uint8_t

Maximum contention window size. Value is calculated from 2^N - 1 where exponent shall be provided as the input. Valid values for exponent N are 0 - 15.

uint8_t

Arbitration Inter-Frame Space Number (AIFSN). Valid range is 0 to 15.

uint8_t

Reserved.

Public Attribute Documentation#

cwmin#

uint8_t sl_wifi_transceiver_cw_config_t::cwmin

Minimum contention window size. Value is calculated from 2^N - 1 where exponent shall be provided as the input. Valid values for exponent N are 0 - 15.


cwmax#

uint8_t sl_wifi_transceiver_cw_config_t::cwmax

Maximum contention window size. Value is calculated from 2^N - 1 where exponent shall be provided as the input. Valid values for exponent N are 0 - 15.


aifsn#

uint8_t sl_wifi_transceiver_cw_config_t::aifsn

Arbitration Inter-Frame Space Number (AIFSN). Valid range is 0 to 15.


reserved#

uint8_t sl_wifi_transceiver_cw_config_t::reserved

Reserved.