Socket Configuration#
The section provides a reference to common socket configuration API function.
Modules#
sl_si91x_socket_type_length_value_t
Functions#
Configures SiWx91x specific socket settings.
Function Documentation#
sl_si91x_config_socket#
sl_status_t sl_si91x_config_socket (sl_si91x_socket_config_t socket_config)
Configures SiWx91x specific socket settings.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_si91x_socket_config_t | [in] | socket_config | Socket configuration of type sl_si91x_socket_config_t. | 
This function sets up the socket configuration specific to the SiWx91x. It must be called before invoking sl_si91x_socket_async. The configuration includes setting parameters such as socket type, protocol, and other options specific to the SiWx91x series.
- Pre-conditions: - Ensure that the necessary initialization for the SiWx91x module has been completed. 
- This API is called before calling sl_si91x_socket_async. 
 
Returns
- sl_status_t. See https://docs.silabs.com/gecko-platform/latest/platform-common/status for details.