Functions#
This section provides a reference to Wi-Fi API functions:
- Common functions to initialize and configure Wi-Fi features. 
- Radio functions to configure the Wi-Fi radio. 
- Scanning functions to scan for Wi-Fi Access Points (APs) in the local area network (LAN). 
- Client functions to implement a Wi-Fi client, otherwise known as a station (STA). 
- Access Point functions to implement a Wi-FI Access Point (AP). 
- Power and Performance functions to configure Wi-Fi connectivity performance. 
- Wi-Fi Protected Setup functions to implement Wi-Fi Protected Setup (WPS). 
- Debugging functions for debugging the Wi-Fi APIs. 
- Wi-Fi Transceiver functions to implement a Wi-Fi Transceiver