Ultra-low-power SRAM (ULP SRAM)#
ULP SRAM is used when the device input is in ultra-low-power mode. SiWG917 has different power domains that are explained in the datasheet. ULP implements multi-port SRAM memory.
Features:
Total 8 KB memory
Total memory divided into four 2K regions.
Access Diagram#
Base addresses for the four 2K banks are as follows (these are Bytewise addresses):
1st 2K: 2406_0000
2nd 2K: 2406_0800
3rd 2K: 2406_1000
4th 2K: 2406_1800
Note: For more information, refer to the SiWG917 Hardware Reference Manual and Datasheet.