You are viewing documentation for version:
PDFStructure to hold the DAC configuration parameters.
Public Attributes#
uint8_t
Operating mode of the DAC.
uint8_t
DAC FIFO threshold level.
uint8_t
ADC channel to be used for the DAC.
uint8_t
DAC pin to be used for the DAC.
uint8_t
DAC port to be used for the DAC.
Public Attribute Documentation#
operating_mode#
uint8_t sl_dac_config_t::operating_mode
Operating mode of the DAC.
dac_fifo_threshold#
uint8_t sl_dac_config_t::dac_fifo_threshold
DAC FIFO threshold level.
adc_channel#
uint8_t sl_dac_config_t::adc_channel
ADC channel to be used for the DAC.
dac_sample_rate#
uint32_t sl_dac_config_t::dac_sample_rate
DAC sample rate.
dac_pin#
uint8_t sl_dac_config_t::dac_pin
DAC pin to be used for the DAC.
dac_port#
uint8_t sl_dac_config_t::dac_port
DAC port to be used for the DAC.