You are viewing documentation for version:
PDFWi-Fi device status structure.
Indicates the status of various Wi-Fi functionalities on the device. It uses bit fields to indicate the status of different Wi-Fi modes and operations.
Public Attributes#
uint8_t
WiFi Access point active.
uint8_t
WiFi promiscuous mode active.
Public Attribute Documentation#
client_active#
uint8_t sl_wifi_status_t::client_active
WiFi Client active.
ap_active#
uint8_t sl_wifi_status_t::ap_active
WiFi Access point active.
monitor_mode_active#
uint8_t sl_wifi_status_t::monitor_mode_active
WiFi promiscuous mode active.
wfd_go_active#
uint8_t sl_wifi_status_t::wfd_go_active
Reserved Status bit.
wfd_client_active#
uint8_t sl_wifi_status_t::wfd_client_active
Reserved Status bit.
scan_active#
uint8_t sl_wifi_status_t::scan_active
Scan in Progress.
_reserved#
uint8_t sl_wifi_status_t::_reserved
Reserved Status bit.
_reserved2#
uint8_t sl_wifi_status_t::_reserved2
Reserved Status bit.