You are viewing documentation for version:
Structure represents the BLE GATT prepare write response.
This structure is used to define the parameters for a BLE GATT prepare write response, which includes the remote device address, the attribute handle, the attribute value offset, the length of the attribute value, and the attribute value itself.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_gatt_prepare_write_response_s::dev_addr[RSI_DEV_ADDR_LEN]
Remote device address
handle#
uint16_t rsi_ble_gatt_prepare_write_response_s::handle
Attribute handle
offset#
uint16_t rsi_ble_gatt_prepare_write_response_s::offset
Attribute value offset
data_len#
uint16_t rsi_ble_gatt_prepare_write_response_s::data_len
Attribute value length
data#
uint8_t rsi_ble_gatt_prepare_write_response_s::data[RSI_DEV_ATT_LEN]
Attribute value (data)