Structure represents the Bluetooth control block.
This structure is used to define the parameters for the Bluetooth control block, which includes status, state, synchronization mechanisms, and remote BLE device information.
Public Attributes#
Public Attribute Documentation#
expected_response_buffer#
void* rsi_bt_cb_s::expected_response_buffer
Driver BT control block expected command response
sync_rsp#
uint8_t rsi_bt_cb_s::sync_rsp
Sync command flag to identify that the command is blocking / sync type
app_buffer_length#
uint32_t rsi_bt_cb_s::app_buffer_length
Buffer length given by application to driver
bt_global_cb#
rsi_bt_global_cb_t* rsi_bt_cb_s::bt_global_cb
Pointer to global Bluetooth callback structure
directed_addr#
uint8_t rsi_bt_cb_s::directed_addr[RSI_DEV_ADDR_LEN]
Address of the device to which directed advertising has to be done in ll privacy mode
remote_ble_info#
rsi_remote_ble_info_t rsi_bt_cb_s::remote_ble_info[MAX_REMOTE_BLE_DEVICES]
Structure holds remote LE device information (BD address and controller buffer availability)
buf_status#
uint8_t rsi_bt_cb_s::buf_status
Variable indicates buffer full/empty status --> 0 -> Empty, 1 -> Full
cmd_status#
uint8_t rsi_bt_cb_s::cmd_status
Variable indicates command in use status --> 0 -> Not In Use, 1 -> In Use
ble_buff_total_avail_cnt#
uint8_t rsi_bt_cb_s::ble_buff_total_avail_cnt
to track total number of available data buffers not based on individual connections
ble_buff_total_mutex#
osMutexId_t rsi_bt_cb_s::ble_buff_total_mutex
Mutex handle for avail_buf_info update