You are viewing documentation for version:
Structure represents the BLE GATT read response.
This structure is used to define the parameters for a BLE GATT read response, which includes the remote device address, the type of the read response, reserved field for future use, the length of the attribute value, and the attribute value itself.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_gatt_read_response_s::dev_addr[RSI_DEV_ADDR_LEN]
Remote device address
type#
uint8_t rsi_ble_gatt_read_response_s::type
Type of the read response
reserved#
uint8_t rsi_ble_gatt_read_response_s::reserved
Reserved for future use
data_len#
uint16_t rsi_ble_gatt_read_response_s::data_len
Attribute value length
data#
uint8_t rsi_ble_gatt_read_response_s::data[RSI_DEV_ATT_LEN]
Attribute value (data)