You are viewing documentation for version:
Structure representing the BLE request for profiles list.
This structure is used to define the parameters for a BLE request to get the profiles list, which includes the remote device address, the handle from which the profiles search would start, and the handle at which the profiles search will stop.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_req_profiles_list_s::dev_addr[RSI_DEV_ADDR_LEN]
Remote device address
start_handle#
uint16_t rsi_ble_req_profiles_list_s::start_handle
Profiles search will start from this handle
end_handle#
uint16_t rsi_ble_req_profiles_list_s::end_handle
Profiles search will stop at this handle