Wi-Fi advanced scan configuration options.
Indicates the configuration parameters for an advanced Wi-Fi scan operation.
Note
active_channel_time and passive_channel_time are applicable for foreground scan (station before connection).
If active_channel_time and passive_channel_time are not set or set to 0, default values are used. Default value of 100 msec is used for active_channel_time when SL_WIFI_DEFAULT_ACTIVE_CHANNEL_SCAN_TIME is passed. Default value of 400 msec is used for passive_channel_time when SL_WIFI_DEFAULT_PASSIVE_CHANNEL_SCAN_TIME is passed.
trigger_level and trigger_level_change are used for automatic roaming functionality. When connected to an AP:
If RSSI drops below trigger_level, a background scan is automatically initiated to find better APs for roaming
If RSSI drops by trigger_level_change delta from the previous measurement, a background scan is triggered
The background scan operates independently and helps facilitate seamless roaming to better APs when available
Public Attributes#
RSSI threshold level to trigger background scan for roaming. When connected to an AP, if the RSSI drops below this level, a background scan is automatically triggered to find better APs for potential roaming.
RSSI delta change threshold to trigger background scan for roaming. If the current RSSI value drops by this delta amount from the previous measurement, a background scan is triggered to find better APs for potential roaming.
Time spent on each channel during active scan (milliseconds)
Time spent on each channel during passive scan (milliseconds)
Flag to start advanced scan immediately.
Flag to send multiple probes to AP. If the value is set to 1, a probe request would be sent to all access points in addition to the connected SSID.
Public Attribute Documentation#
trigger_level#
int32_t sl_wifi_advanced_scan_configuration_t::trigger_level
RSSI threshold level to trigger background scan for roaming. When connected to an AP, if the RSSI drops below this level, a background scan is automatically triggered to find better APs for potential roaming.
trigger_level_change#
uint32_t sl_wifi_advanced_scan_configuration_t::trigger_level_change
RSSI delta change threshold to trigger background scan for roaming. If the current RSSI value drops by this delta amount from the previous measurement, a background scan is triggered to find better APs for potential roaming.
active_channel_time#
uint16_t sl_wifi_advanced_scan_configuration_t::active_channel_time
Time spent on each channel during active scan (milliseconds)
passive_channel_time#
uint16_t sl_wifi_advanced_scan_configuration_t::passive_channel_time
Time spent on each channel during passive scan (milliseconds)
enable_instant_scan#
uint8_t sl_wifi_advanced_scan_configuration_t::enable_instant_scan
Flag to start advanced scan immediately.
enable_multi_probe#
uint8_t sl_wifi_advanced_scan_configuration_t::enable_multi_probe
Flag to send multiple probes to AP. If the value is set to 1, a probe request would be sent to all access points in addition to the connected SSID.