Timeout Configuration Structure.

Public Attributes#

uint16_t

Time spent on each channel when performing active scan (milliseconds). Default value of 100 msec is used when SL_WIFI_DEFAULT_ACTIVE_CHANNEL_SCAN_TIME is passed.

uint16_t

Authentication and association timeout value. Default value of 300 msec is used when SL_WIFI_DEFAULT_AUTH_ASSOCIATION_TIMEOUT is passed.

uint16_t

Keep Alive Timeout value. Default value of 30 seconds is used when SL_WIFI_DEFAULT_KEEP_ALIVE_TIMEOUT is passed.

uint16_t

Time spent on each channel when performing passive scan (milliseconds). The minimum passive_scan_timeout_value is 5 msec, and maximum is 1000 msec. Default value of 400 msec is used when SL_WIFI_DEFAULT_PASSIVE_CHANNEL_SCAN_TIME is passed.

Public Attribute Documentation#

active_chan_scan_timeout_value#

uint16_t sl_wifi_timeout_t::active_chan_scan_timeout_value

Time spent on each channel when performing active scan (milliseconds). Default value of 100 msec is used when SL_WIFI_DEFAULT_ACTIVE_CHANNEL_SCAN_TIME is passed.


auth_assoc_timeout_value#

uint16_t sl_wifi_timeout_t::auth_assoc_timeout_value

Authentication and association timeout value. Default value of 300 msec is used when SL_WIFI_DEFAULT_AUTH_ASSOCIATION_TIMEOUT is passed.


keep_alive_timeout_value#

uint16_t sl_wifi_timeout_t::keep_alive_timeout_value

Keep Alive Timeout value. Default value of 30 seconds is used when SL_WIFI_DEFAULT_KEEP_ALIVE_TIMEOUT is passed.


passive_scan_timeout_value#

uint16_t sl_wifi_timeout_t::passive_scan_timeout_value

Time spent on each channel when performing passive scan (milliseconds). The minimum passive_scan_timeout_value is 5 msec, and maximum is 1000 msec. Default value of 400 msec is used when SL_WIFI_DEFAULT_PASSIVE_CHANNEL_SCAN_TIME is passed.