Wi-Fi Listen interval structure.

Specifies the Wi-Fi Listen interval in milliseconds. The listen interval is the time interval between two consecutive Target Beacon Transmission (TBTT) events. Moving forward, this structure will be deprecated. Instead, use the sl_wifi_listen_interval_v2_t structure. This is retained for backward compatibility.

Public Attributes#

uint32_t

Wi-Fi Listen interval in milliseconds.

Public Attribute Documentation#

listen_interval#

uint32_t sl_wifi_listen_interval_t::listen_interval

Wi-Fi Listen interval in milliseconds.