WiSeConnect - SiWx91x Bluetooth LE SDK Version 4.0.2 (May 4, 2026) - Release Notes#

Wi-Fi 6 + BLE (WiSeConnect) SDK Version 4.0.2

Simplicity SDK Version 2025.12.3

The SiWx91x Bluetooth LE Software Development Kit (SDK) provides feature-rich Bluetooth 5 connectivity with multi-connection capabilities, advanced advertising extensions, and power optimization for diverse IoT applications.

Click here for earlier releases.

Release Summary#

Key Features | API Changes | Bug Fixes | Chip Enablement

Key Features#

Added in 4.0.2#

None

Added in 4.0.1#

None

Added in 4.0.0#

None

API Changes#

Added in 4.0.2#

None

Added in 4.0.1#

None

Added in 4.0.0#

None

Bug Fixes#

Fixed in 4.0.2#

None

Fixed in 4.0.1#

  • Fixed an issue where the output transmit power was higher in end-to-end mode compared to PER test mode across all temperatures.

Fixed in 4.0.0#

  • Resolved multiple BLE issues, including legacy pairing, asynchronous attribute-value handling, incorrect passkey generation, and the WLAN Power Save Disable API.

  • Improved stability and performance by fixing DUT hang conditions, TX notification delays with 10 BLE connections, and issues in dense environments for multi-connection applications.

  • Additional updates include removing unsupported KCC values, fixing the unused NUM_PKTS macro, and resolving local ATT-value failures with variable-length characteristics.

Chip Enablement#

Added in 4.0.2#

  • Added BLE support for SiWX917Y module boards BRD4343C and BRD4357C.

Added in 4.0.1#

None

Added in 4.0.0#

None

Key Features#

New Features | Enhancements | Removed Features | Deprecated Features

Note: See Feature Matrix for a list of any applicable APIs, examples, software variants, modes, hardware, and host interfaces applicable for each feature.

New Features#

Added in 4.0.2#

None

Added in 4.0.1#

None

Added in 4.0.0#

None

Enhancements#

Added in 4.0.2#

None

Added in 4.0.1#

  • Updated the SiWx917 “Update Gain Table” API documentation for better user understanding.

  • Updated the wlan_ble_unified_coex_app README to correct RAM configuration details.

Added in 4.0.0#

  • Reduced active time during extended advertising events to improve power efficiency and performance.

  • Updated BLE synchronous and asynchronous APIs descriptions for improved clarity and accuracy.

  • Updated the description of the SL_SI91X_BT_BLE_STACK_BYPASS_ENABLE macro to clarify that it should only be used with Zephyr.

  • Added additional documentation notes for the RSI_BLE_NUM_REC_BYTES macro in the ble_custom_ext_feature_bit_map configuration to clarify its usage and behavior.

  • Replaced legacy UART APIs with Silicon Labs UART APIs in bt_stack_bypass app.

Removed Features#

Removed in 4.0.2#

None

Removed in 4.0.1#

None

Removed in 4.0.0#

None

Deprecated Features#

Deprecated in 4.0.2#

None

Deprecated in 4.0.1#

None

Deprecated in 4.0.0#

None

API Changes#

New APIs | Modified APIs | Removed APIs | Deprecated APIs

New APIs#

Added in 4.0.2#

None

Added in 4.0.1#

None

Added in 4.0.0#

Modified APIs#

Modified in 4.0.2#

None

Modified in 4.0.1#

None

Modified in 4.0.0#

None

Removed APIs#

Removed in 4.0.2#

None

Removed in 4.0.1#

None

Removed in 4.0.0#

None

Deprecated APIs#

Deprecated in 4.0.2#

None

Deprecated in 4.0.1#

None

Deprecated in 4.0.0#

None

Bug Fixes#

Note: See the Feature Matrix section for a list of all hardware parts that work with the WiSeConnect SDK.

Fixed in 4.0.2#

None

Fixed in 4.0.1#

ID Issue or Limitation Description GitHub / Salesforce Reference (if any) Workaround (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1581271 Updated the SiWx917 "Update Gain Table" API documentation for better user understanding. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1567221 Resolved an issue causing higher BLE transmit power in end-to-end mode versus PER mode across temperatures. This update ensures improved transmit power alignment and regulatory compliance across operating temperatures. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1605174 Updated the wlan_ble_unified_coex_app README to correct RAM configuration details. None None
  • Software variants: Standard
  • OPNs: All except PSRAM OPNs
  • Boards: All applicable boards
  • Modes: SoC
  • Host interfaces: N/A

Fixed in 4.0.0#

ID Issue or Limitation Description GitHub / Salesforce Reference (if any) Workaround (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1543604 Fixed a BLE connection timeout (0x4E08) issue during simultaneous bidirectional TX/RX data transfers of 230 bytes across 10 BLE connections. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1514763 Fixed an issue where BLE legacy pairing failed when the DUT was configured with the 'Keyboard Display' IO capability and the NRF dongle was set to Display YesNo. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1509492 Fixed an issue where rsi_ble_set_att_value_async API fails with a 0x4E60 (Invalid Handle Range) error code when performing connect, disconnect, and reconnection tests with glucose applications. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1497730 Resolved DUT hang occurring after approximately 6 hours during repeated peripheral connect/disconnect cycles while performing TX/RX notifications with 10 BLE connections. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1496803 Fixed an issue where the device delayed TX notifications to a central device by approximately 40-50 seconds when performing simultaneous bidirectional data transfers (TX/RX) with 10 BLE connections. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1465165 Fixed an issue where the device incorrectly generated a passkey during BLE pairing when the initiator (DUT) I/O capability was configured as Keyboard Display and the responder as Display Only. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1516085 Replaced legacy UART API with Silicon Labs UART APIs in the bt_stack_bypass application. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1505006 Removed KCC region values from the BLE IC max power regulatory tables as the devices are not tested for KCC compliance. None None
  • Software variants: Standard and Lite
  • OPNs: All ICs (SiWx917M) only
  • Boards: All ICs (SiWx917M) related boards only
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1516551 Fixed an issue where the NUM_PKTS macro was defined but not used in the BLE PER application. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1506132 Fixed an issue where the rsi_ble_set_local_att_value API returned error code 0x4046 when services were maintained in firmware with the VARIABLE_LENGTH_CHARACTERISTICS feature. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1463443 Fixed an issue where the WLAN Power Save Disable API failed to disable power save mode in the ble_secureconnection_psram application. None None
  • Software variants: Standard and Lite
  • OPNs: PSRAM
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
1488482 Fixed a hang issue that occurred while processing the connection parameter update response command during testing with 10 BLE connections using an encrypted image with both TA and M4 power-save modes enabled. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART

Chip Enablement#

Added in 4.0.2#

None

Added in 4.0.1#

None

Added in 4.0.0#

None

Application Example Changes#

New Examples | Modified Examples | Removed Examples | Deprecated Examples

Note: See the Feature Matrix section for a list of all hardware parts that work with the WiSeConnect SDK.

New Examples#

Added in 4.0.2#

None

Added in 4.0.1#

None

Added in 4.0.0#

None

Modified Examples#

Modified in 4.0.2#

None

Modified in 4.0.1#

None

Modified in 4.0.0#

None

Removed Examples#

Removed in 4.0.2#

None

Removed in 4.0.1#

None

Removed in 4.0.0#

None

Deprecated Examples#

Deprecated in 4.0.2#

None

Deprecated in 4.0.1#

None

Deprecated in 4.0.0#

None

Known Issues and Limitations#

Note: See the Feature Matrix section for a list of all hardware parts that work with the WiSeConnect SDK.

Added in 4.0.2#

None

Added in 4.0.1#

ID Issue or Limitation Description GitHub / Salesforce Reference (if any) Workaround (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1567221 BLE connected power consumption has increased following the transmit power alignment fix. The increase is approximately 8% at the 200ms connection interval and approximately 29% at the 1.28 sec connection interval. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1599776 DUT becomes unresponsive after running BLE TX/RX notifications for more than 5 minutes with power save mode enabled on the 121x board using the ble_unified_ae_coex_app_soc application. None None
  • Software variants: Standard and Lite
  • OPNs: 121x and 141x PSRAM OPNs
  • Boards: All applicable boards
  • Modes: SoC
  • Host interfaces: N/A

Added in 4.0.0#

ID Issue or Limitation Description GitHub / Salesforce Reference (if any) Workaround (if any) Affected Software Variants, Hardware, Modes, Host Interfaces
1504605 For ICs, customers must obtain certification for the required regions. After certification, the corresponding values are loaded through the "BLE – Update Gain Table" APIs. None None
  • Software variants: Standard and Lite
  • OPNs: All except SiW917Y1GN and SiW917Y1GA modules
  • Boards: All applicable boards
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1458618 The ble_data_length application example does not work with 121x and 141x PSRAM OPNs. None None
  • Software variants: Standard and Lite
  • OPNs: 121x and 141x PSRAM OPNs
  • Boards: All applicable boards
  • Modes: SoC
  • Host interfaces: N/A
1465175 The SiWx917 device hangs when power-save mode is enabled during BLE transmit and receive (TX/RX) notifications using the HP chain. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1371967 BLE anchor points were missing during packet exchanges with the PTS dongle when the connection interval (CI) exceeded 960 ms and the supervision latency (SL) was set to 5. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1523829 The minimum supported BLE GATT capability is limited to 4 services and 20 attributes for all memory configurations. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC
  • Host interfaces: N/A
N/A The BLE secondary latency value is valid only up to 32. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
N/A Maximum supported AE data length is 200 bytes. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
N/A Supports only two ADV_EXT sets. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
N/A Supports only two simultaneous BLE connections (either two peripheral, two central, or one central and one peripheral) when Advertising Extensions are enabled. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
N/A System-level changes introduced to enhance stability have resulted in some increase in power numbers (up to 15% for smaller connection interval of 200 ms) for BLE connected only cases for modules only. Impact is smaller for longer connection intervals. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART
1574418 Using slc generate --toolchain gcc or slc generate --with toolchain_gcc might fail with exclusivity errors due to the wiseconnect_toolchain_gcc_standard component incorrectly providing toolchain_gcc, resulting in a conflict with the SiSDK toolchain_gcc component. If using those two command line options results in exclusivity errors, then you can remove them. Note that in a future WiseConnect release, you might have to reintroduce the toolchain option on the command line. Refer to future WiseConnect release notes for updates on possible behavior changes. None None
  • Software variants: Standard and Lite
  • OPNs: All
  • Boards: All
  • Modes: SoC, NCP
  • Host interfaces: SPI, UART