Troubleshooting#

  • For best throughput results, ensure that the AP and server running on the PC are connected over an Ethernet cable.

  • Ensure that IP addresses are assigned to both client and server before running the iPerf test.

  • Ensure that the station is connected to the AP.

  • For running iPerf, the server should first begin listening, and then the client must send the data.