Structure to hold the port and pin of SIO UART.

Public Attributes#

uint8_t

SIO UART TX port.

uint8_t

SIO UART TX pin.

uint8_t

SIO UART TX mux.

uint8_t

SIO UART TX pad.

uint8_t

SIO UART RX port.

uint8_t

SIO UART RX pin.

uint8_t

SIO UART RX mux.

uint8_t

SIO UART RX pad.

Public Attribute Documentation#

uart_tx_port#

uint8_t sl_sio_uart_t::uart_tx_port

SIO UART TX port.


Definition at line 165 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h

uart_tx_pin#

uint8_t sl_sio_uart_t::uart_tx_pin

SIO UART TX pin.


Definition at line 166 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h

uart_tx_mux#

uint8_t sl_sio_uart_t::uart_tx_mux

SIO UART TX mux.


Definition at line 167 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h

uart_tx_pad#

uint8_t sl_sio_uart_t::uart_tx_pad

SIO UART TX pad.


Definition at line 168 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h

uart_rx_port#

uint8_t sl_sio_uart_t::uart_rx_port

SIO UART RX port.


Definition at line 169 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h

uart_rx_pin#

uint8_t sl_sio_uart_t::uart_rx_pin

SIO UART RX pin.


Definition at line 170 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h

uart_rx_mux#

uint8_t sl_sio_uart_t::uart_rx_mux

SIO UART RX mux.


Definition at line 171 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h

uart_rx_pad#

uint8_t sl_sio_uart_t::uart_rx_pad

SIO UART RX pad.


Definition at line 172 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_sio.h