Generic Wi-Fi interface information structure.
Public Attributes#
WLAN state: 1 = connected, 0 = disconnected in station mode; number of stations connected in AP mode.
Channel number of connected AP in station mode; channel number of the module in AP mode.
SSID of connected AP in station mode; SSID of the module in AP mode.
Security type of connected AP is supported in station mode, but not in AP mode.
PSK for AP mode, PMK for station mode.
BSSID address of connected AP in station mode; not supported in AP mode.
Wireless mode used in connected AP (6 - AX, 4 - N, 3 - G, 1 - B) in station mode; not supported in AP mode.
MAC address of the module.
Public Attribute Documentation#
wlan_state#
uint16_t sl_wifi_interface_info_t::wlan_state
WLAN state: 1 = connected, 0 = disconnected in station mode; number of stations connected in AP mode.
channel_number#
uint16_t sl_wifi_interface_info_t::channel_number
Channel number of connected AP in station mode; channel number of the module in AP mode.
ssid#
uint8_t sl_wifi_interface_info_t::ssid[SL_WIFI_SSID_LEN]
SSID of connected AP in station mode; SSID of the module in AP mode.
sec_type#
uint8_t sl_wifi_interface_info_t::sec_type
Security type of connected AP is supported in station mode, but not in AP mode.
psk_pmk#
uint8_t sl_wifi_interface_info_t::psk_pmk[SL_WIFI_MAX_PSK_LENGTH]
PSK for AP mode, PMK for station mode.
bssid#
uint8_t sl_wifi_interface_info_t::bssid[SL_WIFI_BSSID_LENGTH]
BSSID address of connected AP in station mode; not supported in AP mode.
wireless_mode#
uint8_t sl_wifi_interface_info_t::wireless_mode
Wireless mode used in connected AP (6 - AX, 4 - N, 3 - G, 1 - B) in station mode; not supported in AP mode.
mac_address#
uint8_t sl_wifi_interface_info_t::mac_address[SL_WIFI_MAC_ADDRESS_LENGTH]
MAC address of the module.