You are viewing documentation for version:1.0Request message body. Public Attributes#uint32_tsocket_idID of the socket. uint16_tdata_lengthAmount of data to write. uint16_treservedReserved, set to zero. uint8_tdataData to write. Public Attribute Documentation#socket_id#uint32_t sl_wisun_msg_send_on_socket_req_body_t::socket_idID of the socket. data_length#uint16_t sl_wisun_msg_send_on_socket_req_body_t::data_lengthAmount of data to write. reserved#uint16_t sl_wisun_msg_send_on_socket_req_body_t::reservedReserved, set to zero. data#uint8_t sl_wisun_msg_send_on_socket_req_body_t::data[]Data to write.