Indication message body.
Public Attributes#
uint32_t
Status of the indication.
uint32_t
ID of the socket.
uint16_t
Amount of data that can be read.
uint16_t
Reserved, set to zero.
Public Attribute Documentation#
status#
uint32_t sl_wisun_msg_socket_data_available_ind_body_t::status
Status of the indication.
Definition at line
1493
of file protocol/wisun/wisun/inc/sl_wisun_msg_api.h
socket_id#
uint32_t sl_wisun_msg_socket_data_available_ind_body_t::socket_id
ID of the socket.
Definition at line
1495
of file protocol/wisun/wisun/inc/sl_wisun_msg_api.h
data_length#
uint16_t sl_wisun_msg_socket_data_available_ind_body_t::data_length
Amount of data that can be read.
Definition at line
1497
of file protocol/wisun/wisun/inc/sl_wisun_msg_api.h
reserved#
uint16_t sl_wisun_msg_socket_data_available_ind_body_t::reserved
Reserved, set to zero.
Definition at line
1499
of file protocol/wisun/wisun/inc/sl_wisun_msg_api.h