Wi-SUN CoAP descriptor structure.

Public Attribute Documentation#

handler#

sl_wisun_coap_handle_t* sl_wisun_coap::handler

lib handler


Definition at line 98 of file C:/SiliconLabs/SimplicityStudio/v5/developer/sdks/gecko_sdk_suite/v3.2/app/wisun/component/coap/sl_wisun_coap.h

malloc#

sl_wisun_coap_malloc_t sl_wisun_coap::malloc

malloc function


Definition at line 100 of file C:/SiliconLabs/SimplicityStudio/v5/developer/sdks/gecko_sdk_suite/v3.2/app/wisun/component/coap/sl_wisun_coap.h

free#

sl_wisun_coap_free_t sl_wisun_coap::free

free function


Definition at line 102 of file C:/SiliconLabs/SimplicityStudio/v5/developer/sdks/gecko_sdk_suite/v3.2/app/wisun/component/coap/sl_wisun_coap.h

tx_callback#

sl_wisun_coap_tx_callback sl_wisun_coap::tx_callback

TX callback.


Definition at line 104 of file C:/SiliconLabs/SimplicityStudio/v5/developer/sdks/gecko_sdk_suite/v3.2/app/wisun/component/coap/sl_wisun_coap.h

rx_callback#

sl_wisun_coap_rx_callback sl_wisun_coap::rx_callback

RX callback.


Definition at line 106 of file C:/SiliconLabs/SimplicityStudio/v5/developer/sdks/gecko_sdk_suite/v3.2/app/wisun/component/coap/sl_wisun_coap.h

version#

sl_wisun_coap_version_t sl_wisun_coap::version

CoAP version.


Definition at line 108 of file C:/SiliconLabs/SimplicityStudio/v5/developer/sdks/gecko_sdk_suite/v3.2/app/wisun/component/coap/sl_wisun_coap.h