iPerf server header

Public Attributes#

int32_t

Server flag.

uint32_t

Tot bytes rx'd hi part.

uint32_t

Tot bytes rx'd low part.

uint32_t

Stop time in sec.

uint32_t

Stop time in usec.

uint32_t

Lost pkt cnt.

uint32_t

Rx pkt out of order cnt.

uint32_t

Packet count.

uint32_t

Jitter hi.

uint32_t

Jitter low.

Public Attribute Documentation#

dtg#

sl_iperf_udp_datagram_t sl_iperf_udp_srv_hdr::dtg

Udp datagram.


flags#

int32_t sl_iperf_udp_srv_hdr::flags

Server flag.


tot_len_u#

uint32_t sl_iperf_udp_srv_hdr::tot_len_u

Tot bytes rx'd hi part.


tot_len_l#

uint32_t sl_iperf_udp_srv_hdr::tot_len_l

Tot bytes rx'd low part.


stop_sec#

uint32_t sl_iperf_udp_srv_hdr::stop_sec

Stop time in sec.


stop_usec#

uint32_t sl_iperf_udp_srv_hdr::stop_usec

Stop time in usec.


lost_pkt_cnt#

uint32_t sl_iperf_udp_srv_hdr::lost_pkt_cnt

Lost pkt cnt.


out_of_order_cnt#

uint32_t sl_iperf_udp_srv_hdr::out_of_order_cnt

Rx pkt out of order cnt.


packet_cnt#

uint32_t sl_iperf_udp_srv_hdr::packet_cnt

Packet count.


jitter_sec#

uint32_t sl_iperf_udp_srv_hdr::jitter_sec

Jitter hi.


jitter_usec#

uint32_t sl_iperf_udp_srv_hdr::jitter_usec

Jitter low.