Modules#

Type definitions

Over-The-Air Device Firmware Upgrade (Alpha)#

Wi-SUN Over-The-Air Device Firmware Upgrade (OTA DFU) service is implemented for updating Wi-SUN device's firmware. The component uses the Gecko Bootloader API to perform firmware write, verify, and set to bootload operations.

A Trivial File Transfer Protocol (TFTP) client provides downloader solution to obtain a new Gecko Bootloader File (GBL) file from remote host Over-The-Air, using the Wi-SUN network. The connection to the TFTP remote host can be configured in component configuration file. The entire firmware upgrade session can be managed over CoAP. The service includes notification and status request capabilities.

Functions#

void

Initialize the device firmware upgrade service.

sl_status_t

Start firmware update.

sl_status_t

Stop firmware update.

uint32_t

Get the status value.

const char *

Get the status string in JSON format.

void

Free the status string buffer.

bool
sl_wisun_ota_dfu_get_fw_update_status_flag(const sl_wisun_ota_dfu_status_t status_flag)

Get the status flag value.

void
sl_wisun_ota_dfu_error_hnd(const sl_wisun_ota_dfu_error_code_t error_code, sl_wisun_ota_dfu_error_ctx_t *const ctx)

OTA DFU error handler (weak implementation)

Function Documentation#

sl_wisun_ota_dfu_init#

void sl_wisun_ota_dfu_init (void )

Initialize the device firmware upgrade service.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Initialize Wi-SUN OTA Device Firmware Upgrade service.


sl_wisun_ota_dfu_start_fw_update#

sl_status_t sl_wisun_ota_dfu_start_fw_update (void )

Start firmware update.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Start firmware update by setting SL_WISUN_OTA_DFU_STATUS_FW_UPDATE_STARTED flag Returns

  • sl_status_t SL_STATUS_OK on success, otherwise SL_STATUS_FAIL


sl_wisun_ota_dfu_stop_fw_update#

sl_status_t sl_wisun_ota_dfu_stop_fw_update (void )

Stop firmware update.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Stop firmware update by setting SL_WISUN_OTA_DFU_STATUS_FW_UPDATE_STOPPED flag Returns

  • sl_status_t SL_STATUS_OK on success, otherwise SL_STATUS_FAIL


sl_wisun_ota_dfu_get_fw_update_status#

uint32_t sl_wisun_ota_dfu_get_fw_update_status (void )

Get the status value.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returning the value of event flags Returns

  • uint32_t Status


sl_wisun_ota_dfu_get_fw_update_status_json_str#

const char * sl_wisun_ota_dfu_get_fw_update_status_json_str (void )

Get the status string in JSON format.

Parameters
TypeDirectionArgument NameDescription
voidN/A

String buffer is allocated in heap by CoAP allocator Returns

  • const char * Allocated string pointer on success, otherwise NULL


sl_wisun_ota_dfu_free_fw_update_status_json_str#

void sl_wisun_ota_dfu_free_fw_update_status_json_str (const char * str)

Free the status string buffer.

Parameters
TypeDirectionArgument NameDescription
const char *[in]str

String ptr

Call CoAP free to release allocated memory


sl_wisun_ota_dfu_get_fw_update_status_flag#

bool sl_wisun_ota_dfu_get_fw_update_status_flag (const sl_wisun_ota_dfu_status_t status_flag)

Get the status flag value.

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_ota_dfu_status_t[in]status_flag

Status flag enum

Bool representation of status variable bit value Returns

  • bool true if the flag is set, otherwise false


sl_wisun_ota_dfu_error_hnd#

void sl_wisun_ota_dfu_error_hnd (const sl_wisun_ota_dfu_error_code_t error_code, sl_wisun_ota_dfu_error_ctx_t *const ctx)

OTA DFU error handler (weak implementation)

Parameters
TypeDirectionArgument NameDescription
const sl_wisun_ota_dfu_error_code_t[in]error_code

Error code

sl_wisun_ota_dfu_error_ctx_t *const[in]ctx

Error context with error details

Catch error in different stages of boot load.