Util Functions#

The Util Functions component provides helper functions to inform the application about the Wi-SUN PHY configured in the RAIL configuration file.

Functions#

sl_status_t
sl_wisun_util_get_rf_settings(uint8_t *reg_domain, uint8_t *op_class, uint16_t *op_mode) SL_DEPRECATED_API_SDK_4_2

Get frequency band settings of the first RAIL configuration listed in RAIL's channelConfigs array.

sl_status_t
sl_wisun_util_get_phy_config(sl_wisun_phy_config_t *phy_config)

Get PHY settings of the first RAIL configuration listed in RAIL's channelConfigs array.

sl_status_t
sl_wisun_util_connect(const uint8_t *network_name)

Connect to a Wi-SUN network.

Function Documentation#

sl_wisun_util_get_rf_settings#

sl_status_t sl_wisun_util_get_rf_settings (uint8_t * reg_domain, uint8_t * op_class, uint16_t * op_mode)

Get frequency band settings of the first RAIL configuration listed in RAIL's channelConfigs array.

Parameters
TypeDirectionArgument NameDescription
uint8_t *[out]reg_domain

Regulatory domain of the Wi-SUN network

uint8_t *[out]op_class

Operational class of the Wi-SUN network

uint16_t *[out]op_mode

Operational mode of the Wi-SUN network

Returns

  • SL_STATUS_OK if successful, an error code otherwise

Warnings

  • Do not call this function while the Wi-SUN stack is started.

DeprecatedThis function will be removed in the future versions of the Wi-SUN stack. See sl_wisun_util_get_phy_config() for a replacement.


sl_wisun_util_get_phy_config#

sl_status_t sl_wisun_util_get_phy_config (sl_wisun_phy_config_t * phy_config)

Get PHY settings of the first RAIL configuration listed in RAIL's channelConfigs array.

Parameters
TypeDirectionArgument NameDescription
sl_wisun_phy_config_t *[out]phy_config

Pointer to PHY configuration

Returns

  • SL_STATUS_OK if successful, an error code otherwise

Warnings

  • Do not call this function while the Wi-SUN stack is started.


sl_wisun_util_connect#

sl_status_t sl_wisun_util_connect (const uint8_t * network_name)

Connect to a Wi-SUN network.

Parameters
TypeDirectionArgument NameDescription
const uint8_t *[in]network_name

Name of the Wi-SUN network as a zero-terminated string

Returns

  • SL_STATUS_OK if successful, an error code otherwise

Since Wi-SUN frequency band settings are deduced from first RAIL configuration listed in RAIL's channelConfigs array, using this function is not recommended if more than one RAIL configuration is described.