LFN network parameters.

Public Attributes#

uint16_t

Address registration lifetime (IPv6 lease duration) the LFN requires to the Border Router (minutes).

uint8_t

Duration for which an LFN waits for a registration confirmation (minutes).

uint8_t

Reserved, set to zero.

Public Attribute Documentation#

lfn_registration_lifetime_m#

uint16_t sl_wisun_lfn_params_network_t::lfn_registration_lifetime_m

Address registration lifetime (IPv6 lease duration) the LFN requires to the Border Router (minutes).

Specification range [1440, 5040]


Definition at line 87 of file /mnt/raid/workspaces/ws.x49WyIS5n/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h

lfn_na_wait_duration_m#

uint8_t sl_wisun_lfn_params_network_t::lfn_na_wait_duration_m

Duration for which an LFN waits for a registration confirmation (minutes).

Specification range [30, 120]


Definition at line 90 of file /mnt/raid/workspaces/ws.x49WyIS5n/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h

reserved#

uint8_t sl_wisun_lfn_params_network_t::reserved

Reserved, set to zero.


Definition at line 92 of file /mnt/raid/workspaces/ws.x49WyIS5n/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h