Authentication parameter set.
Public Attributes#
Security protocol trickle timer.
PMK lifetime (minutes)
PTK lifetime (minutes)
Security protocol retry timeout (seconds)
Initial EAPOL-Key first Tx min delay (seconds)
Initial EAPOL-Key first Tx max delay (seconds)
Initial EAPOL-Key retry exponential backoff min (seconds)
Initial EAPOL-Key retry exponential backoff max (seconds)
Initial EAPOL-Key retry exponential backoff max limit (seconds)
Temporary neighbor link minimum timeout (seconds)
GTK_REQUEST_IMIN (minutes)
GTK_REQUEST_IMAX (minutes)
GTK_MAX_MISMATCH (minutes)
LGTK_MAX_MISMATCH (minutes)
Security protocol trickle timer expirations.
Initial EAPOL-Key retry limit.
If true, allow join state 2 to be skipped using cached credentials from the previous connection.
Reserved, set to zero.
Public Attribute Documentation#
sec_prot_trickle#
sl_wisun_trickle_params_t sl_wisun_params_eapol::sec_prot_trickle
Security protocol trickle timer.
sec_prot_retry_timeout_s#
uint16_t sl_wisun_params_eapol::sec_prot_retry_timeout_s
Security protocol retry timeout (seconds)
initial_key_min_s#
uint16_t sl_wisun_params_eapol::initial_key_min_s
Initial EAPOL-Key first Tx min delay (seconds)
initial_key_max_s#
uint16_t sl_wisun_params_eapol::initial_key_max_s
Initial EAPOL-Key first Tx max delay (seconds)
initial_key_retry_min_s#
uint16_t sl_wisun_params_eapol::initial_key_retry_min_s
Initial EAPOL-Key retry exponential backoff min (seconds)
initial_key_retry_max_s#
uint16_t sl_wisun_params_eapol::initial_key_retry_max_s
Initial EAPOL-Key retry exponential backoff max (seconds)
initial_key_retry_max_limit_s#
uint16_t sl_wisun_params_eapol::initial_key_retry_max_limit_s
Initial EAPOL-Key retry exponential backoff max limit (seconds)
temp_min_timeout_s#
uint16_t sl_wisun_params_eapol::temp_min_timeout_s
Temporary neighbor link minimum timeout (seconds)
sec_prot_trickle_expirations#
uint8_t sl_wisun_params_eapol::sec_prot_trickle_expirations
Security protocol trickle timer expirations.
initial_key_retry_limit#
uint8_t sl_wisun_params_eapol::initial_key_retry_limit
Initial EAPOL-Key retry limit.
allow_skip#
uint8_t sl_wisun_params_eapol::allow_skip
If true, allow join state 2 to be skipped using cached credentials from the previous connection.