Custom FSK PHY configuration.

Public Attributes#

uint32_t

Ch0 center frequency in kHz.

uint16_t

Channel spacing in kHz.

uint16_t

Number of channels.

uint8_t

PHY mode ID.

uint8_t
uint8_t

FSK preamble length in bits.

uint8_t

Reserved, set to zero.

Public Attribute Documentation#

ch0_frequency_khz#

uint32_t sl_wisun_phy_config_custom_fsk_t::ch0_frequency_khz

Ch0 center frequency in kHz.


channel_spacing_khz#

uint16_t sl_wisun_phy_config_custom_fsk_t::channel_spacing_khz

Channel spacing in kHz.


number_of_channels#

uint16_t sl_wisun_phy_config_custom_fsk_t::number_of_channels

Number of channels.


phy_mode_id#

uint8_t sl_wisun_phy_config_custom_fsk_t::phy_mode_id

PHY mode ID.


crc_type#

uint8_t sl_wisun_phy_config_custom_fsk_t::crc_type

FSK CRC type (sl_wisun_crc_type_t)


preamble_length#

uint8_t sl_wisun_phy_config_custom_fsk_t::preamble_length

FSK preamble length in bits.


reserved#

uint8_t sl_wisun_phy_config_custom_fsk_t::reserved[1]

Reserved, set to zero.