You are viewing documentation for version:1.9.0Trickle parameter set. Public Attributes#uint16_timin_sMinimum interval size (seconds) uint16_timax_sMaximum interval size (seconds) uint8_tkRedundancy constant (0 for infinity) uint8_treservedReserved, set to zero. Public Attribute Documentation#imin_s#uint16_t sl_wisun_trickle_params_t::imin_sMinimum interval size (seconds) imax_s#uint16_t sl_wisun_trickle_params_t::imax_sMaximum interval size (seconds) k#uint8_t sl_wisun_trickle_params_t::kRedundancy constant (0 for infinity) reserved#uint8_t sl_wisun_trickle_params_t::reserved[3]Reserved, set to zero.