Explicit PHY configuration.
Public Attributes#
uint32_t
Ch0 center frequency in kHz.
uint8_t
Specifies the set of channels on which the device is permitted to transmit.
uint8_t
Channel spacing (sl_wisun_channel_spacing_t)
uint16_t
Number of channels.
uint8_t
PHY mode ID.
Public Attribute Documentation#
ch0_frequency_khz#
uint32_t sl_wisun_phy_config_explicit_t::ch0_frequency_khz
Ch0 center frequency in kHz.
channel_mask#
uint8_t sl_wisun_phy_config_explicit_t::channel_mask[SL_WISUN_CHANNEL_MASK_SIZE]
Specifies the set of channels on which the device is permitted to transmit.
This mask applies to asynchronous (PAS, PA, ...), unicast and broadcast frames. The channel mask is advertised in both US-IE and BS-IE elements.
channel_spacing#
uint8_t sl_wisun_phy_config_explicit_t::channel_spacing
Channel spacing (sl_wisun_channel_spacing_t)