You are viewing documentation for version:
Adaptive rate algorithm rate stats.
Public Attributes#
uint16_t
Number of tx without acknowledgement.
int8_t
Indicates if the rate can be probed.
uint32_t
Number of times the rate was selected.
uint8_t
Number of times this rate was skipped.
uint16_t
Number of successful transmissions.
float
Estimated chance of success.
float
Estimated throughput in kb/s.
Public Attribute Documentation#
fail_count#
uint16_t sl_wisun_rate_stats_t::fail_count
Number of tx without acknowledgement.
frame_duration_us#
uint32_t sl_wisun_rate_stats_t::frame_duration_us
Frame tx time.
probe_limit#
int8_t sl_wisun_rate_stats_t::probe_limit
Indicates if the rate can be probed.
reserved#
uint8_t sl_wisun_rate_stats_t::reserved[2]
Reserved, set to zero.
sample_count#
uint32_t sl_wisun_rate_stats_t::sample_count
Number of times the rate was selected.
skipped_sample_count#
uint8_t sl_wisun_rate_stats_t::skipped_sample_count
Number of times this rate was skipped.
success_count#
uint16_t sl_wisun_rate_stats_t::success_count
Number of successful transmissions.
success_probability#
float sl_wisun_rate_stats_t::success_probability
Estimated chance of success.
throughput#
float sl_wisun_rate_stats_t::throughput
Estimated throughput in kb/s.