Ping info structure type definition.

Public Attributes#

uint16_t

Identifier.

bool

Lost packet flag.

uint16_t

ICMPv6 packet length including header.

Wi-SUN remote address.

uint32_t

Response time millisecond.

uint16_t

Sequence number.

uint32_t

Start time stamp.

uint32_t

Stop time stamp.

Public Attribute Documentation#

identifier#

uint16_t sl_wisun_ping_info::identifier

Identifier.


Definition at line 111 of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h

lost#

bool sl_wisun_ping_info::lost

Lost packet flag.


Definition at line 125 of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h

packet_length#

uint16_t sl_wisun_ping_info::packet_length

ICMPv6 packet length including header.


Definition at line 115 of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h

remote_addr#

sockaddr_in6_t sl_wisun_ping_info::remote_addr

Wi-SUN remote address.


Definition at line 119 of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h

response_time_ms#

uint32_t sl_wisun_ping_info::response_time_ms

Response time millisecond.


Definition at line 117 of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h

sequence_number#

uint16_t sl_wisun_ping_info::sequence_number

Sequence number.


Definition at line 113 of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h

start_time_stamp#

uint32_t sl_wisun_ping_info::start_time_stamp

Start time stamp.


Definition at line 121 of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h

stop_time_stamp#

uint32_t sl_wisun_ping_info::stop_time_stamp

Stop time stamp.


Definition at line 123 of file /mnt/raid/workspaces/ws.G6qn92p5B/overlay/gsdk/app/wisun/component/ping/sl_wisun_ping.h