iPerf log type definition

Public Attributes#

Buff string instance.

bool

Buffered.

bool

Colored.

int32_t

Last result.

int32_t(*

Stdout and buffer printer.

Public Attribute Documentation#

buff#

sl_iperf_log_str_buff_t sl_iperf_log::buff

Buff string instance.


Definition at line 270 of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

buffered#

bool sl_iperf_log::buffered

Buffered.


Definition at line 264 of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

colored#

bool sl_iperf_log::colored

Colored.


Definition at line 262 of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

last_res#

int32_t sl_iperf_log::last_res

Last result.


Definition at line 266 of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h

print#

int32_t(* sl_iperf_log::print) (struct sl_iperf_log *const log, const char *format,...)

Stdout and buffer printer.


Definition at line 268 of file /mnt/raid/workspaces/ws.wIWINzxl8/overlay/gsdk/app/wisun/component/iperf/sl_iperf_types.h