Request message body.

Public Attributes#

uint16_t

number of rates available in the array space

Neighbor MAC address.

uint8_t

Reserved, set to zero.

Public Attribute Documentation#

allocated_rate_count#

uint16_t sl_wisun_msg_get_rate_algorithm_stats_id_req_body_t::allocated_rate_count

number of rates available in the array space


neighbor#

sl_wisun_mac_address_t sl_wisun_msg_get_rate_algorithm_stats_id_req_body_t::neighbor

Neighbor MAC address.


reserved#

uint8_t sl_wisun_msg_get_rate_algorithm_stats_id_req_body_t::reserved[2]

Reserved, set to zero.