Confirmation message body.
Public Attributes#
uint16_t
Number of rates copied.
Neighbor MAC addresses read.
uint8_t
Reserved, set to zero.
uint32_t
Status of the request.
Public Attribute Documentation#
rate_count#
uint16_t sl_wisun_msg_get_rate_algorithm_stats_cnf_body_t::rate_count
Number of rates copied.
rates#
sl_wisun_rate_t sl_wisun_msg_get_rate_algorithm_stats_cnf_body_t::rates[]
Neighbor MAC addresses read.
reserved#
uint8_t sl_wisun_msg_get_rate_algorithm_stats_cnf_body_t::reserved[2]
Reserved, set to zero.