You are viewing documentation for version:
PDFAdaptive rate algorithm rates.
Public Attributes#
uint8_t
Rate index on the rate list.
uint8_t
Indicates if rate is supported by both the node and the neighbor.
uint8_t
Maximum amount of retries with current rate.
Struct containing the rate's tx statistics.
Public Attribute Documentation#
index#
uint8_t sl_wisun_rate_t::index
Rate index on the rate list.
is_supported#
uint8_t sl_wisun_rate_t::is_supported
Indicates if rate is supported by both the node and the neighbor.
max_retries#
uint8_t sl_wisun_rate_t::max_retries
Maximum amount of retries with current rate.
phy_mode_id#
uint8_t sl_wisun_rate_t::phy_mode_id
Rate phy mode id.
rate#
uint32_t sl_wisun_rate_t::rate
Rate in kb/s.
stats#
sl_wisun_rate_stats_t sl_wisun_rate_t::stats
Struct containing the rate's tx statistics.