MPL parameter set.
Public Attributes#
uint8_t
MPL seed-id type, 0 indicates the seed-id is elided and is the IPv6 source address, 3 indicates the seed-id is the 128-bit ULA/GUA of the source.
uint16_t
MPL seed set entry lifetime (seconds)
MPL trickle timer.
uint8_t
MPL trickle timer expirations.
Public Attribute Documentation#
seed_id_type#
uint8_t sl_wisun_params_mpl_s::seed_id_type
MPL seed-id type, 0 indicates the seed-id is elided and is the IPv6 source address, 3 indicates the seed-id is the 128-bit ULA/GUA of the source.
Definition at line
239
of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
seed_set_entry_lifetime_s#
uint16_t sl_wisun_params_mpl_s::seed_set_entry_lifetime_s
MPL seed set entry lifetime (seconds)
Definition at line
233
of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
trickle#
sl_wisun_trickle_params_t sl_wisun_params_mpl_s::trickle
MPL trickle timer.
Definition at line
231
of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
trickle_expirations#
uint8_t sl_wisun_params_mpl_s::trickle_expirations
MPL trickle timer expirations.
Definition at line
235
of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h