MPL parameter set.

Public Attributes#

uint8_t

Reserved, set to zero.

uint16_t

MPL seed set entry lifetime.

Warning: MPL parameters may be overwritten for border router MPL trickle timer.

uint8_t

MPL trickle timer expirations.

Public Attribute Documentation#

reserved#

uint8_t sl_wisun_br_params_mpl_s::reserved

Reserved, set to zero.


Definition at line 146 of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_connection_params_api.h

seed_set_entry_lifetime_s#

uint16_t sl_wisun_br_params_mpl_s::seed_set_entry_lifetime_s

MPL seed set entry lifetime.


Definition at line 142 of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_connection_params_api.h

trickle#

sl_wisun_trickle_params_t sl_wisun_br_params_mpl_s::trickle

Warning: MPL parameters may be overwritten for border router MPL trickle timer.


Definition at line 140 of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_connection_params_api.h

trickle_expirations#

uint8_t sl_wisun_br_params_mpl_s::trickle_expirations

MPL trickle timer expirations.


Definition at line 144 of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/border_router/sl_wisun_br_connection_params_api.h